Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Super Thin-Shaped Magic Band

Super Thin-Shaped Magic Band
Sales Price: 4.99 SGD
Review Rating: 2.40
5 Customer Reviews
5 star 1
4 star 1
3 star 0
2 star 0
1 star 3
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Bundle the code
1
From Japan
On 2015-08-15 16:01:14
Magic itself is good. The edges of the tape (both sides and cut) are easy to unravel, and when unwinding many times, it will be a little easy. Suitable for applications that do not remove once wound.
This review is about item#09143513.
Used to bundle LAN wiring
5
From Japan
On 2015-02-25 14:30:27
Until now, we used cheap ones, but when we bundle about 3 in the thin type, the edges turned over but the "Kuraray" made things never turn and it is easy to work It is.
This review is about item#09143495.
Bundle wiring
1
From Japan
On 2013-11-18 20:27:56
The advantage is that the disadvantages of being thin and easy to cut are as follows: 1) When you remove it many times, the end comes in. ② Can not sew on clothing etc. (Because the tape is thin, it will tear from the seams)
This review is about item#09143513.
Cable wiring for LAN etc.
4
From Japan
On 2012-04-23 13:45:23
It is good to use it only once, but it is not recommended for continuous use (for temporary fixation). Thin but vibration? Since it is weak to, etc., it fixes it to be long. I am satisfied if it only fixes at this price.
This review is about item#09143513.
Wiring bundle
1
From Japan
On 2012-01-28 01:46:41
Unlike ordinary velcro, it is a very thin tape. It is unsuitable for repeated use because the cotton part is durable. It is suitable for applications that do not remove it while bundling it.
This review is about item#09143513.
1
Customer Who Viewed This Item Also Viewed
Double Sided Hook Loop
Hook and Loop Fastener,
Double Sided Hook Loop
Flexible Belt, Band
Binding Tape
Aspire Packaging Tape
Mix Flower
Hook and Loop Fastener
Magic Band
Magic Band