Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of HSS high-speed steel hole saw

HSS high-speed steel hole saw
Sales Price: 19.99 SGD
Review Rating: 3.40
5 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Processing sheet metal
5
From Japan
On 2015-02-17 13:08:36
It was used for hole punching of 2 mm aluminum plate. I was able to smoothly puncture it with sharpness. I am satisfied.
This review is about item#09145875.
hole
5
From Japan
On 2014-03-15 01:31:47
I bought it for drilling of wood. I thought it would be possible to open it easily with steel plates.
This review is about item#09145771.
Drilling of thin steel plate
1
From Japan
On 2013-10-09 18:48:35
The sharpness is very good, but the cut material can not be removed from Holso - and it is hard to use.
This review is about item#09145543.
Drilling into thin plate materials
5
From Japan
On 2011-06-01 21:46:04
Veneer and tin board are common. · · Rain water accumulates in the waste radial AG tire (lug tire for tractor) which was used as a stand of the working machine instead of the gantry of the working machine, so it is used for other purposes, so water is added to the sidewall part (with thread thickness of 15 mm) Try opening a hole! I went up easy and beautifully! However, I think that it is impossible for the bead or tread portion containing the steel wire. If I take a rubber plate slowly, is it enough to get a thickness of 30 millimeters? It is!
This review is about item#09145936.
Drilling of aluminum die-casting plate
1
From Japan
On 2011-06-01 21:26:09
Although it may be impossible for a 12 mm hole saw, since the center drill is as thick as 6 mm, the aluminum bite stops biting into teeth. You can not use it unless you remove aluminum that sticks one by one.
This review is about item#09145534.
1
Customer Who Viewed This Item Also Viewed
Bimetal hole saw
E type hole cutter (SKH51)
HSS Hole Saw
Bimetal Hole Saw
Bimetal Hole Saw J Shaped
Z Hole Saw
(90980) HOUSING, CONNECTOR