Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hand Lap, Glass, Pump Dispenser

Hand Lap, Glass, Pump Dispenser
Sales Price: 15.99 SGD
Review Rating: 2.43
7 Customer Reviews
5 star 1
4 star 2
3 star 0
2 star 0
1 star 4
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
At base correction
1
From Japan
On 2018-02-08 10:48:23
Foundation Correction Flux cleaning alcohol was put in and used, but siphoning was worse than when it arrived but it got up when pushing it dozens of times, so I used it for the time being, but after 3 months it does not rise at all and it becomes useless It was. I contacted the customer and asked for a replacement but it was not contacted and I am in contact with the selling agency (AS ONE). It is a shame that I will not be able to respond when I bought it.
This review is about item#9155124.
Degreasing work (using gasoline)
1
From Japan
On 2017-03-10 21:52:30
It is good to stop with the first "click" when the outer cap is a two-stage type, but it will be great if you can not remove it if you set it all the way back. In order to remove it you have to pull out to force to prepare to spill the contents. Because the tube length is short, the "usable amount of liquid" is small, and you have to add it with chocolate chocolate. Because it is bad usability, I purchase another product that will enter about 300 CC and use it.
This review is about item#9155124.
For cleaning the electronic board
4
From Japan
On 2016-11-03 18:56:19
I use anhydrous ethanol but it is very convenient to use without problems. Although the cap snaps in, it feels like a little hard.
This review is about item#9155124.
Removal of solvent for wiping operation
4
From Japan
On 2013-12-26 16:16:38
Mostly satisfactory. Originally, when trying to remove the outer cap from the bottle, the catch with the bottle body was too large, it was very difficult to remove. I wanted to improve this point because it was just fine as it scraped off the bulge inside the outer cap with a cutter knife. The inner tube does not reach the bottom of the bottle has design intent and is meaningful and does it? I want to be improved if it is just a design mistake.
This review is about item#09155124.
Cleaning before printing.
1
From Japan
On 2011-08-23 22:00:29
When putting benzine, the resin part will crack a few days later and it will not be used. Because it is impossible to return it, it can not be done either.
When cleaning alcohol
5
From Japan
On 2010-11-19 11:07:43
It is convenient because you can use both hands. Although I was a bit uneasy looking at the review, I can use it without problems.
Used for solvents such as printed circuit board flux removal solution
1
From Japan
On 2010-08-29 02:37:11
The tube is short (it does not reach the bottom), and it can not be sucked if the liquid volume is low. I want the cap to be screw type. If the inner cap is loose, liquid is scattered when removing the cap. Inner cap is easy to loosen. After purchasing one, I purchased two additional, but one of the latter two, the inner cap quickly loosens, one is that the inner cap screws are stupid and can not be used, after all the second two Not available.
This review is about item#09155124.
1
Customer Who Viewed This Item Also Viewed
Hand Lap, Pump Dispenser
FINE Hand Lap Glass, Pump Dispenser 300mL
Wash bottle with label
Hand wrap
Hand wrap (made by PFA)
Saw Handle
Hand Lap, Glass, Pump Dispenser
Hand wrap SCC
Solvent Dispenser Bottles
Polyethylene Hand Lap, Pump Dispenser
Clean Pot
One Touch Pot
Hand Lap, Glass, Pump Dispenser