Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Cusion Drill For Iron work

Cusion Drill For Iron work
Sales Price: 5.99 SGD
Review Rating: 4.75
8 Customer Reviews
5 star 6
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Installation work of wooden and aluminum push edges on window glass
5
From Japan
On 2018-02-22 19:24:17
I used it for pilot holes of fine screws, but it is very solid and can be used with confidence.
This review is about item#9523534.
Drilling drill
4
From Japan
On 2018-01-04 21:43:34
It is the second purchase. This time I bought two books. Because it is cheap, I will purchase it when I need it.
This review is about item#9523534.
Construction
5
From Japan
On 2017-05-29 18:48:48
I do not quite understand the comparison with others, but the appearance and design were good.
This review is about item#9171522.
Drilling
4
From Japan
On 2016-06-27 18:29:50
I understood the meaning of the cushion. I feel that it became easier to pierce holes.
This review is about item#10006911.
Drilling
5
From Japan
On 2015-12-27 07:27:13
Although it is color coded by size, I think that it would be better to color-code more finely. It is because presbyopia can not see numbers if it is similar size.
This review is about item#10006945.
4mm tap pilot hole
5
From Japan
On 2015-03-04 19:12:32
Because there is a cushion, it is hard to break, sharpness is also the best.
This review is about item#09171531.
Light metal processing
5
From Japan
On 2014-04-04 21:14:23
The balance between pricing and use feeling is wonderful. Main parts to be used may be aluminum and compatibility may be good.
This review is about item#09523561.
Drilling of general metal
5
From Japan
On 2012-05-12 13:00:16
It is a sharpness not ashamed of the name of Bessel. Just because I miss the tip, I do not recommend using impact.
This review is about item#09523613.
1