Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Rotor

Rotor
Sales Price: 2.99 SGD
Review Rating: 4.57
7 Customer Reviews
5 star 6
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
For stirring experiment
5
From Japan
On 2017-03-27 16:39:58
unused. Preliminary observation of rotatability with a magnetic stirrer.
This review is about item#9203634.
Beaker prototype
5
From Japan
On 2016-04-18 00:27:06
I think that it is suitable for 50 ml, 100 ml beaker. I think that it can be used even in a 200 ml beaker. When it becomes 300 ml beaker or more, stirring efficiency will increase for 40 mm length and 50 mm length. However, if the length is too close to the diameter of the beaker, the rotation will not be smooth and the stirring efficiency will be lower, so be careful.
This review is about item#09203634.
Used for stirring in brine electrolysis beaker test
5
From Japan
On 2014-07-04 15:34:07
As a electrolytic cell, we used a 7 L aquarium for goldfish polystyrol. Set the temperature to 50 ° C and stir with a 8φ X 50 L rotor. It was confirmed that the fine bubbles (hydrogen and oxygen) generated in the electrode were dispersed throughout and well agitated. However, after the end of the experiment, a circle of concentric circle scratches was formed at the position where the rotor at the bottom of the container was rotating. It is not the rotor's responsibility because the material of the aquarium is a problem, but it was the point I noticed. For example, it may be good to lay a "cushion" under the rotor.
This review is about item#09203634.
Agitation of liquid agent
5
From Japan
On 2014-04-18 16:57:46
It was very good
This review is about item#09203616.
Stirring process of soil analysis
2
From Japan
On 2014-04-07 14:10:26
Although there is no problem with respect to magnetic force, the coating on the surface was easily scraped off during the use process, and this floating material was generated in the water and I was in trouble.
This review is about item#09203652.
Agitation of chemicals
5
From Japan
On 2014-03-16 15:49:20
I am satisfied with using it without problems.
This review is about item#09203591.
Used for stirring dyes
5
From Japan
On 2013-10-28 16:50:49
It can be used without problems. Since the price is cheap, I bought it to be free shipping together with other items. Monotaro is saved because there are many goods.
This review is about item#09203625.
1
Customer Who Viewed This Item Also Viewed
Octagon Rotor
PTFE Court Stirrer
Lab Run Rotor
Oval Stirring Bar
Octagon Rotor
Stirring Bar Wheel Shape
Fine Stirrer
Stirring Bar
Octagonal Spinbar, Teflon
Mini Stirrer
Cross Head Rotor Double
Triangle Rotor
Micro-rotor
Stirrer gear type
Rotor (value set)
PTFE stirrer
PTFE Stirrer Bar