Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Branch Joint for Drain Hoses

Branch Joint for Drain Hoses
Sales Price: 3.99 SGD
Review Rating: 3.40
5 Customer Reviews
5 star 1
4 star 1
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Outdoor unit
3
From Japan
On 2018-04-17 20:16:41
I used it regularly, so I will do it again because it is a husband
This review is about item#32979046.
Exchange when branch joint breakage
3
From Japan
On 2018-02-15 11:50:46
Is it difficult to insert the hose into the hose insertion port, can not you comply with all manufacturers
This review is about item#32979046.
Veranda air conditioning drain hose plumbing
4
From Japan
On 2017-10-28 14:57:29
I used it not for vertical arrangement but for horizontal arrangement. I wanted a simple Y shape but I bought it because there was only one seller.
This review is about item#32979046.
"Measures to prevent rain from the veranda floor board"
5
From Japan
On 2015-05-18 22:09:32
It is used for "measures against rain from the veranda floor board". It is a small, inexpensive and convenient part for packing the drain hose from two places into one, though it uses an air conditioning drain hose because it is too big for parts for the rain gutter. Since the drain hose uses thing made by Inaba Electric Works, connection is also securely connected.
This review is about item#32979046.
Connection of indoor unit and outdoor unit for drainage hose for air conditioner
2
From Japan
On 2013-11-20 22:01:38
The combination with the φ14 drain hose on hand (not made in Inaba) was bad and it did not stabilize. Since it fits into the drainage hose made by Inaba (φ16) indeed, there is no problem with the product itself. At the home center level, since φ 14 is large, I thought it would be better if I could connect them smoothly.
This review is about item#32979046.
1
Customer Who Viewed This Item Also Viewed
Rotation Type Total Counter
Pan drainage flexible
Sink Drainage Plug Y Hose, Threaded
T type cheese for drain pipe
Sink Drainage Hose Y Coupler
Hose for Sink
Drain Hose VP Joint
Magnet door contact
Anhydrous warm cabinet
Pan drainage flexible
Drain branch joint
Drain Hose Y
Drain Hose Joint
Drain Hose for Sink
Branch Joint Y