Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of SDS Plus Bit S4

SDS Plus Bit S4
Sales Price: 26.99 SGD
Review Rating: 5.00
7 Customer Reviews
5 star 7
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Drilling of anchor beating
From Japan
On 2017-02-20 17:35:58
Piercing speed is higher than ordinary concrete bit, and it is satisfied in a short time
This review is about item#6683756.
Chemical anchor hole
From Japan
On 2016-10-18 20:32:57
There is no problem at all as it is drilled in concrete as a manufacturer product at all, there are cases where the home center is cheap in terms of price, but in the case of purchase when purchasing at discount there are also cases where it is inexpensive and it is very convenient for expense processing is there
This review is about item#10009806.
Used for drilling concrete and granite
From Japan
On 2015-10-27 19:27:11
Since the discharge of dust is quick and the blade also breaks, work is quick. I think that it is better than those of other companies.
This review is about item#06683783.
Concrete drilling
From Japan
On 2015-03-22 21:30:08
You can drill precisely. I think that it is difficult to use it all the time because it is a cutting edge consumable item ... I think that life expectancy is different depending on the number of times to open a deck etc.
This review is about item#06683905.
Used when penetrating concrete
From Japan
On 2014-03-06 22:56:16
We use it when penetrating concrete. I am very satisfied with excellent price sharpness.
This review is about item#06683756.
Termite control work
From Japan
On 2013-05-09 14:05:09
The drilling work of the concrete became easier and the shoulder had been avoided until now, but the burden of feeling was alleviated.
This review is about item#06683896.
I will cast an anchor bolt on the wall of an apartment with renovation work.
From Japan
On 2011-07-08 19:22:41
The SDS plus bit is handy for easy exchange of cones by hand. When there is work to drill holes in the steel plate, not only in concrete, there are times when the circular cone gets idled. If SDS plus bit, there is absolutely no idling so workability is good. For hexagonal awls for concrete, it is necessary to prepare two drills and workability is bad.
This review is about item#10064661.