Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Air Hose

Air Hose
Sales Price: 68.99 SGD
Review Rating: 4.80
10 Customer Reviews
5 star 8
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
It is used for pressure welding work.
5
From Japan
On 2017-09-28 15:34:29
Since the hose runs behind the ceiling of the factory, the horizontal line of the hose is very helpful for replacement work.
This review is about item#9233314.
For wooden road construction nailing
4
From Japan
On 2017-08-04 15:04:39
The hose is too soft and a bit uneasy, so anxious at break
This review is about item#9233314.
Car maintenance
5
From Japan
On 2017-05-21 10:28:31
The coupler lock mechanism is occasionally troublesome although it is light and easy to use for both couplers and hoses that do not have curling habits
This review is about item#9233314.
Use of air tools
4
From Japan
On 2017-01-08 17:24:48
The hose feels good, it looks easy to use. It was not displayed at the time of the search, it was displayed at the same time as it was bought at the same time after confirming the order and added order. If ordered on the day it will not cost shipping fee, although it is a free shipping item even if it is a single item, I think that if you can choose it at the time of selection (search) if possible. Star-1 is an impression of the specification of the search system, and the item is a star full mark for items.
This review is about item#9233332.
When cleaning the machine
5
From Japan
On 2016-09-30 18:52:31
It is easy to use and convenient. I hope the hose does not bend.
This review is about item#9233323.
Formwork fabrication
5
From Japan
On 2016-05-19 11:26:45
It is very supple and easy to use.
This review is about item#09233332.
Car maintenance
5
From Japan
On 2015-06-29 15:19:17
It is more flexible than I thought, it will not break even if bent.
This review is about item#09233314.
In the garage
5
From Japan
On 2015-01-20 08:21:43
Domestic hose has supple.
This review is about item#09233314.
Tire replacement etc. Automobile maintenance
5
From Japan
On 2014-11-19 16:12:23
It can be used very smoothly. There is no breakage or entanglement of the hose, etc. It is very helpful at the time of the movement, for example. Also, the hose itself is very light, couplers etc. are lightly easy to handle.
This review is about item#09233314.
Manual work in factory
5
From Japan
On 2011-12-08 16:20:11
It is a product that is more than a price that is very comfortable to use, we were using an inexpensive air hose, but it was replaced quickly, this time with an air hose. Satisfaction is a perfect score.
This review is about item#09233323.
1
Customer Who Viewed This Item Also Viewed
Polyurethane Hose
Suntec Air Hose
Air Hose Clear
Air Hose
Air Hose, With One-Touch Coupler
Alpha Urethane Hose
Quattro air hose