Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Carbide 4 Flute End Mill With Tialn Coating

Carbide 4 Flute End Mill With Tialn Coating
Sales Price: -
Review Rating: 4.49
41 Customer Reviews
5 star 30
4 star 5
3 star 3
2 star 2
1 star 1
The reviews are automatic translation.
Showing 1 - 20 of 41 Reviews
Instead of router bits
5
From Japan
On 2016-08-11 19:41:08
It will cut better than a bit for woodworking. The sound is also quiet, it does not fit in the spiral bit as expected, but this one is better than the straight bit, I also bought a Mitsubishi made end mill with a high price, but obviously here (monotaro brand) It is better to cut. Why?
This review is about item#9241181.
Rough cutting with CNC milling number on desk
4
From Japan
On 2016-05-13 02:49:39
It is perfect for sharpness, rigidity and life span. As you can say for the end mill of Monotaro in general, but the making of it is weak and you can break it quickly. I hope it is a case with a little more strength ....
This review is about item#09241163.
Use for finishing to cut grooves
4
From Japan
On 2015-09-11 22:15:22
I hope there are more kinds / there is a fine size
This review is about item#09241154.
metal
5
From Japan
On 2015-06-18 20:49:42
Cospa is very good, other sizes are also being considered for repeated purchase.
This review is about item#09241197.
Side cutting of aluminum material
5
From Japan
On 2015-04-26 15:58:22
We cut off the side of the general aluminum material of thickness 6 mm by about 2 mm thickness. It was able to be cut smoothly without feeling resistance, and the cutting surface was also beautiful. I did not cut out, drill holes, or cut iron, so I do not know the sharpness in the real sense, but the feeling of use was satisfactory enough.
This review is about item#09241172.
Puncture
1
From Japan
On 2015-01-22 21:25:21
Although I bought it before, I used it for the first time, not to puncture a hole in lauan wood, but if I draw a shallow line as a mark of drilling, I broke it in half in 5 minutes and it was a defective item.
This review is about item#09241127.
Aluminum plate t10 circle hollow, brass square material width 20 mm depth 20 mm groove
5
From Japan
On 2014-10-08 22:53:35
The surface is also beautiful after cutting it smoothly.
This review is about item#09241154.
General-purpose, wooden framework
5
From Japan
On 2014-08-07 22:42:35
I have been using the flash bit up to now, but first of all the noise became surprisingly small as a comparison. Although it is still used only as pine laminated wood, the chipping near the king mouth has decreased. It seems likely to be able to process at low speed so we wanted variable speed trimmer quickly.
This review is about item#09241163.
Used for railroad model
5
From Japan
On 2014-03-27 17:22:12
You can cut well. Processing is easy.
This review is about item#09241127.
It is used for cutting iron, aluminum, stain
3
From Japan
On 2014-03-21 10:55:02
Although there is usually no problem, we hope to have something with a little rake and also raffin, please examine it!
This review is about item#09241145.
Model steam locomotive policy
5
From Japan
On 2014-02-11 13:13:28
I always purchase the same type. The sharpness of the blade lasted long and I am very satisfied.
This review is about item#09241172.
2017 cutting
4
From Japan
On 2013-04-18 20:09:36
I think cutting edge is prone to breakage, but breakage is satisfactory. I feel that the consumption of the coat is quicker than I expected. But as a consumable good enough to be convinced.
This review is about item#09241172.
Cutting and edge polishing of aluminum substrate and acrylic substrate
5
From Japan
On 2013-03-31 18:18:12
Very tight flavor is good. Although it is waiting for arrival of acrylic dedicated end mill now, since it is in good condition also, it is under review again.
This review is about item#09241127.
Woodworking work at the router
5
From Japan
On 2013-03-18 20:40:46
You can cut well. Although durability is obviously still unknown yet, I think that it is a satisfactory quality if you consider it as a consumable item as others say.
This review is about item#09241163.
Planar cutting of aluminum
5
From Japan
On 2013-03-18 19:51:05
It was more pleasant sharpness than I expected.
This review is about item#09241163.
For woodworking trimmer
5
From Japan
On 2012-11-23 20:43:43
It is satisfactory with sharpness and cost performance. Compared to the straight bit for the trimmer, the sharpness is good and the sound is quiet as well. Recommended for those who are considering similar usage.
This review is about item#09241163.
Ferrite bonded magnet plate processing
5
From Japan
On 2012-11-20 11:52:27
A 6 mm diameter carbide end mill was used for drilling and perimeter processing to a magnet plate thickness of 2 mm. This time it was 26 pieces of 677 holes per A4 size. Because it is a cheap end mill, it was thought that there was damage to the cutting edge, probably immediately because it is a ceramic and resin kneaded product mainly composed of ferrite powder. . . I was deeply moved with no astonishing damage. We also bought first-class makers' items and used them as spares, but they were not used. Thank you Mr. Monotaro! I decided to continue purchasing. There was not a loss of money purchase.
This review is about item#09241163.
Planar cutting of A7075 material
2
From Japan
On 2012-11-05 21:00:40
The sharpness is good or just once used, the coating of one of the four blades has been peeled off. It is a product whose durability remains doubt by prioritizing sharpness. In other manufacturers, there was not such a thing.
This review is about item#09241181.
Planar cutting of aluminum parts
3
From Japan
On 2012-10-30 21:16:54
Although I am very satisfied with sharpness, peeling of the coating and small cracks occurred in one of the four teeth after finishing one aluminum part. There was no such thing with other well-known manufacturers, so I would like you to exchange them if possible.
This review is about item#09241181.
Precision Machine Protective Cover Shavings
5
From Japan
On 2012-10-16 16:15:11
Sharpness is also good and workability smooth
This review is about item#09241145.
1 2 3