Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of V-Beltk Type, Standard

V-Beltk Type, Standard
Sales Price: 6.99 SGD
Review Rating: 4.56
34 Customer Reviews
5 star 27
4 star 3
3 star 2
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 20 of 34 Reviews
Used for desktop lathes
5
From Japan
On 2018-05-22 14:53:38
I do appreciate the lot of goods of Monotaro because we do not sell very thin v-belts
This review is about item#9245695.
On the drill press
5
From Japan
On 2018-02-06 15:23:53
Where the V belt which was hardened and deteriorated was exchanged, the sound became quiet and vibration almost disappeared. I think that it is reasonable and very good product.
This review is about item#9245747.
For handmade woodworking lathes
5
From Japan
On 2018-01-13 11:01:21
I am satisfied that it is light, easy to use and comfortable to handle with the thing as desired.
This review is about item#9245731.
Three-roller loaded belt with load
5
From Japan
On 2017-11-20 17:06:51
I exchanged because the belt deteriorated because of the load of three poster rollers. After installation, the load that had deteriorated and became light became original. Because the price is also cheap, I would like to exchange regularly in the future as well.
This review is about item#35968484.
For electrical equipment
3
From Japan
On 2017-10-26 15:41:54
I was sick of trying it lazily Well, I think.
This review is about item#9245792.
Panasonic dryer
5
From Japan
On 2017-09-01 20:50:04
We placed an order in place of the production finished parts. It was awfully awesome.
This review is about item#9245887.
Machine remodeling
4
From Japan
On 2017-07-18 16:00:33
I am satisfied with the cost. It is not used for a long time, but it is also excellent with no abnormal wear.
This review is about item#35968493.
Small lathe power belt.
5
From Japan
On 2017-05-22 14:41:23
Manufacturer's genuine replacement parts (same standard) price is also high and high, it is necessary for several weeks to place orders. I am saved.
This review is about item#9245695.
I changed the spindle's axis, so I bought it for replacement.
1
From Japan
On 2016-12-23 20:17:58
Although there is no problem with the product, it did not understand the size of the belt, it was purchased as an estimate, so it was longer than I thought, then K40 was a little longer then K39, just Just Fit (eventually purchased 3 sizes). It may be useful if there is a guide table of the belt size or a calculation formula.
This review is about item#9245896.
Belt change of tabletop drilling machine
4
From Japan
On 2016-08-05 08:11:21
Because vibration of M base desk drilling board TB131 is large and it is hard to make a change, I tried changing the belt. The attached one is K28.5 which is very difficult to obtain with extremely dimensions and therefore purchased K28 and K29. In K28, the tension was strong and vibrations increased conversely. Although the tension is loose in K29, you can use it if you adjust your eyes by adjustment. Vibration is about to receive a somewhat reduced feeling. I wonder why M company adopted a belt difficult to obtain. It seems that the accuracy of the old drilling machine was better. The belt of K29 is a good product and it does not matter.
This review is about item#09245765.
Maintenance of machine tools
5
From Japan
On 2016-05-05 15:07:11
It is very helpful to rural areas because it is hard to come by surprise.
This review is about item#09245695.
For driving a car air conditioner
5
From Japan
On 2016-03-17 13:44:02
Used for driving self-made car air conditioners. There is also durability, it is saved because it was available cheaply.
This review is about item#09245914.
Pure belt of Makita's drilling machine came up and purchased for replacement.
1
From Japan
On 2016-01-27 23:58:17
Because someone reviewed the same Makita drilling machine using a three-star belt and heard that the vibration sound was improved, I also purchased two lengths of V-belt K 28 and K 29 to see for myself trying, I tried to adjust the tension, etc., but I was not able to use the vibration and the sound greatly in any length though it attempted to adjust the tension with a short to the belt. By the way, the length of the genuine belt is 28.5 inches, and the three-star belt does not have this length.
This review is about item#09245774.
For three loading device of roller.
5
From Japan
On 2015-12-17 09:21:25
Although the genuine belt was bad, this item also has durability and can be used still more.
This review is about item#35968484.
On the motor pulley
5
From Japan
On 2015-11-24 16:38:32
I have never compared it with other companies' products, but I can use it well enough A little more explanation display is easy to understand and it is saved I am ordering 2 sizes by size difference
This review is about item#09245905.
Specification for vacuum pump (automobile)
5
From Japan
On 2015-10-14 09:35:20
V - belt handling store has no stock and purchased this time. It is also a very good product which also fits to the pulley diameter
This review is about item#35968493.
Machine overhaul
5
From Japan
On 2015-07-06 15:48:43
Especially it was able to be used without problems.
This review is about item#35092057.
Refurbishment of desktop drills
5
From Japan
On 2015-05-30 22:01:46
We got a domestic brand desk drill which was already discontinued. The belt cured by aging and decided to replace it. We found the same part number in your company catalog, and it is instant delivery status in stock. At the same time we ordered the bearings and finished maintenance of the desk drills in a short period of time. I am very happy that I was able to acquire and exchange belts made of long-time beloved three-star brand.
This review is about item#09245765.
Net winding
5
From Japan
On 2015-04-03 11:28:58
I did not deal with nearby shop, correspondence was early and it was saved.
This review is about item#35968493.
By drilling machine
3
From Japan
On 2015-03-25 13:33:55
There is no problem with both product and price
This review is about item#09245747.
1 2
Customer Who Viewed This Item Also Viewed
V-Belt Standard M Type
V-Belt Standard K Type
V Belt
V-belt M type (standard)
V Belt,
V Belt M Type, Red
V-Belt A Type, Standard
V BELT M RED
Lock Nut
Plate (clutch) 13089-1085
Polyurethane Belt,Polly Max 5M Type
Sewing Machine Belts