Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of 50 mm of Webbing Sling Width

50 mm of Webbing Sling Width
Sales Price: 51.71 SGD
Review Rating: 4.00
6 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Steel transport
5
From Japan
On 2017-05-29 08:56:29
Color coding is very good. It is easy to understand and well received by the site.
This review is about item#08414235.
During can making work
1
From Japan
On 2016-12-27 17:14:48
Although there was also a precautionary note, as you said, "If you slide on the edge it will cut off" As you say about 1.5 tons of suspended workpiece pulled inside with a laser, I think that it is probably about 5, 60 cm, but if you slip and roll Corner pads cut along with product falls. It happened to be a low place so there was no damage other than sling. Do not overconcure corner putt for belt sling. (There are also deficiencies in how to hang) Do not use one that you do not use.
This review is about item#8414253.
Fishing gear on processed product
3
From Japan
On 2016-10-19 16:35:08
When it is used for about two years, it unexpectedly fits. If you lose 1 piece and buy it by 1 piece, the length is quite different.
This review is about item#8414323.
Car Wrecker
5
From Japan
On 2013-07-25 17:45:05
I am satisfied with the item and I am satisfied with the amount of money. I would like to ask dealings in the future as well.
This review is about item#08414244.
Unloading related to equipment, for unloading
5
From Japan
On 2013-07-04 14:18:38
It is soft and easy to use. There is a size chart affixed, it is handy to look for items of how the item number.
This review is about item#08414244.
Triangular hook in the factory
5
From Japan
On 2013-06-13 15:24:51
Shipment window 2 Used for loading steel materials with triangular hooks at the factory. Since coloring is made to two colors, loading can be done smoothly, and colors are conspicuous, so convenience is good in a dark factory. The price is slightly higher compared to other companies.
This review is about item#08414253.
1
Customer Who Viewed This Item Also Viewed
Polyester Sling
Belt Sling BSL Type
Wide Soft Sling
Belt Sling 75mm Width
Corner Pat
Belt Sling / NB III E
Web Sling
Eye-And-Eye Polyester Sling
Eye-And-Eye Belt Slings
Belt Sling
Belt Sling NBIIIE
Inca lifting sling JIS
Eye-And-Eye Belt Sling
Nylon Sling