Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Free Stop Hinge

Free Stop Hinge
Sales Price: 6.99 SGD
Review Rating: 4.83
6 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Light legs
From Japan
On 2017-07-02 16:23:54
With the torque of the eyes firmly, it was perfect for the purpose of use. very good.
This review is about item#9324165.
Bathroom vanity top mirror mounting BOX, features of a folding counter on which the top board extends
From Japan
On 2014-07-06 08:20:55
At first, I was worried about whether it could be used firmly, but when load was applied, it moved smoothly and it gets in any position, so I found a very good hardware and I was impressed with the carpenter.
This review is about item#09324122.
Electric box
From Japan
On 2014-06-05 21:43:56
I am satisfied with the item as expected.
This review is about item#09324165.
It is used as angle adjustment of small speaker stand and wall mounting · ceiling mounting metal fittings.
From Japan
On 2013-11-12 15:20:39
It is very convenient for angle adjustment of small speakers. This free stop hinge is a perfect product to use for our small speaker, it is compact and light, making it simple design possible. The strength of the hinge is neither hard nor soft when used for small products. Since we use it for angle adjustment, it is troubled if the adjusted speaker just moves by touching the music vibration or chot, and it is hard when you try to adjust the angle, so it will be troublesome to break the walls and ceiling so hard I use it conveniently. Although it may be impossible, I tried low temperature baking painting once I tried painting it once I made it possible to make a freeze top hinge that can be baked, once it was damaged.
This review is about item#09324165.
From Japan
On 2013-09-05 23:17:09
There was a request to wear a sliding door that can be opened and closed on the ceiling, I bought two pieces. It seems that the sliding door was heavy and I could not open it if I could not open it at around 85 degrees. I think I will order two more in addition.
This review is about item#09324113.
Acrylic work parts
From Japan
On 2012-02-01 17:29:09
I am satisfied. The hinge is harder than I thought, in the series I bought the one with the smallest size, and if there is no leverage, I need considerable strength. If the attached side is a weak material, it may crack when a force to cause a hinge is added. This time I used it as a part of acrylic work · · box lid ·. At first I was planning to stop two, but because it was too powerful I changed it to 1 sheet.
This review is about item#09324165.
Customer Who Viewed This Item Also Viewed
Free Stop Hinge, Hinge Only
Free Stop Hinge
Free Stop Hinge, Flat Type
Rising Hinge Piece
Free Stop Hinge
Hinge With Stopper
Stay for The Upper Lid