Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Luxury Metalwork Jig Saw Blade

Luxury Metalwork Jig Saw Blade
Sales Price: 3.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Thin sheet metalworking manual sawing saw - electric jig saw
5
From Japan
On 2018-01-27 10:20:41
I was able to meet again with the best quality. Although we mainly use electric powered thread saws, we used a variety of commercially available thread saw blades for metalworking but so far it was not easy to cut and the blade was cutting out soon. The saw blade I had separately from the experts of the goldworker was precisely saved before long but it is a place where the obtaining route was constantly in trouble. Recently, precision machining was necessary, purchasing a manual jigsaw, at the same time I bought this yarn saw blade at the same time It was exactly the same feeling of use as the precision thread saw blade I used beforehand, the tooth sharpness and lifespan were impressed for a long time. It is exactly eyes from the eyes. If you say selfish hope, it will be easier to set it on electric powered thread saw if the total length is 10 to 20 mm longer.
This review is about item#9426715.
Cutting operation
3
From Japan
On 2017-09-13 21:28:51
As of now, it can be used without breaking. In case Sharpness is good. It is convenient and very useful.
This review is about item#9426715.
Thin plate processing
5
From Japan
On 2016-04-21 10:22:58
After purchasing it thought that it was domestic, it was a little surprising though the contents were made in Germany. It is thin compared with the thread saw replacement blade sold at the hardware store around there anyway. I was worried so I tried out, but I did not have to worry about cutting, I was easy to turn around because of slimness, I thought this was nice. Because it is a cheap frame, I thought that it is something I would like to use with a higher frame.
This review is about item#09426715.
Born carving production
5
From Japan
On 2014-05-24 13:37:11
It is good and it is very good,
1