Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Raincoat Work

Raincoat Work
Sales Price: 87.99 SGD
Review Rating: 3.71
7 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
When washing outer walls of condominiums
5
From Japan
On 2018-01-27 19:19:52
Anyway it is a strong durable wrap It is a reinforced work and works hard to recover the garbage collected in the drain of the balcony, but it is hard to wear out which is hard to wear out of course it is hard to wear boots, but you can adjust the hem well, you can firmly adjust the hem 180 cm Slender and L size is just fine
This review is about item#9433365.
It is used in the work of the ship.
4
From Japan
On 2015-12-10 15:43:05
It is light because it is easy to work even if you wear it in the rain, I think that it is good because moisture does not accumulate on the inside.
This review is about item#09433365.
Landscaping
2
From Japan
On 2015-02-18 07:13:56
I used it for landscaping and pruning work for about two years and bought a third thing. Workability is extremely good, such as hem squeezing and mobility, but there is somewhat a problem with strength. Although the outerwear lasts for a long time, the lower trousers burn out without having a half year or more (the sewn portion on the inside of the knees varies vertically) Encourage durability or strongly hope for separate selling separately.
Working on scaffoldings and roofs
4
From Japan
On 2013-11-23 22:22:28
As I just bought it and I have not used it only at work, so far as I noticed. It is better to have a dedicated container (bag) of fabric similar to Katafu. I am diverting prefilled containers that I used before. It is better to take the length of the velcro at the bottom of the lower wing more lengthy for both the male and female to make the adjustment width more than it is now. There are times when you are wearing socks and ordinary shoes, and there are times when you use it with tightening the boots from the top with wearing boots. In the case of myself, when wearing this Temp. Wearing Tabi, I exceeded the effect range of the Velcro, I could not tighten the hem. (I bought it based on the displayed height, so I do not think that it is too big) I think that the point made sturdier, such as reinforcement of the knee, is pretty good.
This review is about item#09433541.
On-site work on rainy days
1
From Japan
On 2012-02-12 22:56:10
Although I bought a vigorously high wing, I bought it for a month after buying it, but it has broken along the crease of the seam allowance of the reinforced part of the knee, although I only wear it on rainy days. it's awful!
This review is about item#09433401.
Lift operation in factory
5
From Japan
On 2010-03-15 15:18:27
It is hard to enter rainwater and it is recommended that it is not steamed.
This review is about item#09433347.
I use it for high-pressure cleaning of the building's outer wall.
5
From Japan
On 2009-01-11 18:16:04
As it is a work on the scaffolding, it is often kappa that is hooked on a line or the like, but this is durable. Expensive Gore-Tex is also strong, but for field use · · ·.
This review is about item#09433487.
1
Customer Who Viewed This Item Also Viewed
Rainwear, Pegasus
Safety Rainwear
B-10 Rain Suit
Pro Safety Rainsuit
Rain Strong Alpha, Camouflage
Rain Overalls
Rain Strong
3D Breeze Rain
Rain Suit
Rainwear Libra, Libeler
Rain Suit
Rain Suit
Rainware,
Rainwear, Takumi