Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Soft PVC Hose, "SUPER TOYORON HOSE", ST-9

Soft PVC Hose, "SUPER TOYORON HOSE", ST-9
Sales Price: 8.99 SGD
Review Rating: 5.00
4 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
As a hose of a car oil tank
5
From Japan
On 2017-03-09 13:45:00
It meets the conditions of high pressure resistance, oil use, endurance temperature, transparent material, low price. It means that it is a long life, and those with an inner diameter of 9 are thick and do not have dents unless they are bent extremely. It's hard to pinch so it's hard to pinch. I could just plug it in to the hose of inner diameter fitting the outer shape 15 without any joint and just clasp it. The hardness of this hose was useful because the inner diameter becomes smaller further when the joint is attached.
This review is about item#37610867.
Air hose
5
From Japan
On 2016-05-02 15:43:15
It is strong and supple. It is a very good item.
This review is about item#37610851.
Used for oil hose.
5
From Japan
On 2015-10-29 13:53:39
There is hardness to some extent, even if the hose is bent to a steep angle it is hard to be crushed and it is strong, it is very good. It is the best dish for applications that require strength.
This review is about item#09483686.
ATF exchange
5
From Japan
On 2012-10-18 16:21:30
The material may also be soft
This review is about item#37610867.
1