Customer Reviews of Fixed for O And S Type, Nbr
The reviews are automatic translation.
Showing 1 - 20 of 51 Reviews
Carburetor repair

From Japan
On 2018-04-24 21:04:39
I used it for repairing the carburetor. Size setting was abundant too and it was saved.
This review is about item#9512212.
When fishing rod maintenance

From Japan
On 2018-04-16 21:10:33
As a result of examining the size,
I reached this part, it was perfect size.
This review is about item#9511844.
Leak tightness

From Japan
On 2018-03-11 21:14:33
I used it for a leak-proof. It is good that the performance is high.
This review is about item#9512212.
Motorcycle also repaired

From Japan
On 2018-03-03 10:34:36
It is oil resistant and is used as a substitute at about one fifth of genuine parts. Because it is a rubber part, it is more economical to exchange every opportunity than to use genuine old parts carefully, and there is no trouble due to deterioration.
This review is about item#9512237.
For hermetic sealing of machine

From Japan
On 2018-03-01 08:03:11
Since you can check the size on the site, you can rest assured that many types of products can be confirmed on the screen without making an order mistake so it is safe. I always appreciate it.
This review is about item#09512291.
WA Gaba magazine gas leak repair

From Japan
On 2018-02-20 15:03:33
I was able to fix it much cheaper than the manufacturer.
This review is about item#09512115.
Work parts for industrial high school work.

From Japan
On 2018-01-29 17:59:04
I purchased it because it is compatible with small lot and kind.
This review is about item#9512081.
On occasion maintenance

From Japan
On 2018-01-20 15:22:09
I used it for replacing old goods.
Currently, it is running without problems.
This review is about item#9511826.
Used for LED light

From Japan
On 2017-12-06 00:05:51
Unfortunately I used it for o-ring of LED light but unfortunately the wire diameter can not be used with ss size
This review is about item#9511896.
To repair toy gun

From Japan
On 2017-12-02 19:27:07
Toy gun (due to gas leaks in gas magazine magazine) Purchased for repair. It is saved because it can purchase from 1 piece. Today the repair is completed.
This review is about item#9512045.
DT 125 repair 35 years ago

From Japan
On 2017-11-06 22:55:20
I was able to finally find compatible products with various sizes abundantly. I did not sell it at home centers etc. I was saved.
This review is about item#9511941.
Hand shower head repair

From Japan
On 2017-10-16 18:59:05
It fits perfectly. Because the ring got stuck with multiple heads.
This review is about item#9511896.
Repair of gas gun

From Japan
On 2017-10-11 15:21:27
I used it for the O ring of the rear end of the floating valve of Western Arms. It was perfect.
This review is about item#9511686.
Motorbike restoration

From Japan
On 2017-10-02 19:40:52
I used it as a seal in the fuel cock. I'm a bit too thick or my cook is getting harder but I will see how it is going. If you do not understand, I will buy a little thin one so I will try that. Because unit price is cheap, we can buy a lot and try it.
This review is about item#9511932.
Car Maintenance

From Japan
On 2017-07-02 15:57:09
Monotaro is thankful for delivering even one order. There is a certain merchant claiming that even one piece is free for shipping, but I will take the commission for the reason I do not understand the translation. I can not forgive them.
This review is about item#9512167.
Packing of water purifier

From Japan
On 2017-06-22 16:59:18
O - ring that was in the old type water purifier cartridge receiving part was broken by deterioration, and I was looking for it. In the home center, the wire diameter was 2.4 mm which was the lowest and it was scraped by me, but it did not work, I found out this. It is perfect for linear 1.5 mm, and there is no water leak. It was good that we could also purchase reserve.
This review is about item#9511844.
Power generator function

From Japan
On 2017-06-14 16:28:01
Thank you for your prompt delivery. It was functional enough.
This review is about item#9511871.
During machine maintenance

From Japan
On 2017-06-07 23:32:17
When overhauling the machine Replace the O ring. It is easy to organize because it is contained in a bag with one piece and one piece number written, but I would like you to enlarge the letters a little more.
This review is about item#9511871.
Bike carburetor OH

From Japan
On 2017-05-28 17:20:54
It can be purchased from 1 piece Even a genuine shortage will manage somehow Carburetor revived
This review is about item#9512167.
Repair of air tools

From Japan
On 2017-04-13 23:03:24
It is a tool that was concerned about air leakage, but packing was broken after disassembling. There, Monotaro! Rare size is also available so it is useful. After replacing the packing, it worked perfectly without problems and the torque seems to have increased.
This review is about item#9511896.