Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hexagon-head axis puncturing

Hexagon-head axis puncturing
Sales Price: 8.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 5
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
When blind hole is processed
5
From Japan
On 2018-02-18 01:45:07
If you do not need precision enough to use the end mill, you can use it very easily.
This review is about item#09536387.
Making fishing tackle
5
From Japan
On 2015-09-10 22:01:42
It is a very good product.
This review is about item#09516701.
Thin drilling operation
4
From Japan
On 2014-10-13 17:50:02
I have polished myself for about 30 years ago how to grind this edge. Although it is possible to make round hole drilling like the metal core, the shape of the cutting edge also shows a larger diameter more prominently. However, it is very regrettable that there is only a thin dust.
This review is about item#09516726.
Drilling of quenched ribbon steel
4
From Japan
On 2014-05-25 11:32:29
For ordinary drill blades for aluminum alloys, free cutting steels, etc., 0.5t hardened blade will be useless in one time when used for ribbon steel. It is cheap for cost though I want you to have a little more because it opens neatly with good skill with this hole and holds about 5 times. Shank does not have to be hexagon so if you can make it cheap you want the previous straight out.
This review is about item#09516683.
Aluminum square pipe (thickness 2 mm)
5
From Japan
On 2013-10-05 19:55:17
Bali got out a little, but a beautiful hole opened easily. I would like to try using different sizes.
This review is about item#09516823.
Used for processing aluminum
5
From Japan
On 2012-10-28 15:26:09
Although I was thinking that I wanted to use it from the front, I tried to purchase because the product under presently needs precision. Was it still good? I mark it with a punch for manual work, but it will definitely have a hole on that street. It is natural, but it is staggering compared to what we have done so far. The hole is also beautiful. If the price is another cheap one, we would like to arrange things of other thickness, but we will keep it at the size we need now.
This review is about item#09516753.
Processing of aluminum materials for jigs
5
From Japan
On 2010-09-30 19:40:11
It may be the best way to not get out of the position of the punch. Because it cuts like Fossner bit, the speed is not fast, but a beautiful round hole opens. I would like to stock each size if the price is cheaper a little.
This review is about item#09516866.
1
Customer Who Viewed This Item Also Viewed
Spot Drill
Hexagon-head axis ironworking twist drill
No. 6 multiuse bit
Plate Pal Drill
Drill Bit
Well drilling
Triangular drill (10 type)