Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Ratchet Rivet Gun

Ratchet Rivet Gun
Sales Price: 129.99 SGD
Review Rating: 2.83
6 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 3
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Installation of hall seat cushion rubber
5
From Japan
On 2015-01-09 14:02:03
As I looked at the review "I can not use it at all or I am not a defective product", so I posted it. I have been using it for nearly two years, but it is perfectly a nice item. Especially if the stainless rivet is not this gun, the shaft can not be cut even if applying a large force, but with this product it can be cut with a light force, if the correct axis is also operated, it falls out with the pollory.
This review is about item#10009562.
Kitchen sheet metal attachment
1
From Japan
On 2012-04-14 09:37:59
I used the same rivetter gun from old days but this new rivetter gun can not be used at all It is not a defect This rivetter gun is not defective I will exchange it, but I also bought three of my acquaintance dealers, but I am also afraid that they can not be used at all I think that I have not inspected whether it can be used properly
This review is about item#10009562.
It is a repost.
5
From Japan
On 2011-07-14 09:33:27
It became manufacturer's returned goods, it returned on inspection of each part. I am in good health.
This review is about item#10009562.
Track Body
1
From Japan
On 2011-06-28 15:45:10
I have a bad start from the first one. Even if you release the lever while you are hitting and trying to redraw it again, the ratchet does not return and can not be redrawn. Even if ratchets are occasionally free, next time rivets jump out forward and can not be pulled. After struggling to struggle somehow, trying to eject the remaining core from behind, this time just chewing and do not leave, only the core will return backwards ahead. Everything is amusing, it does not become totally usable. I'm not sure if it is broken, or whether the compatibility of the rivet and nosepiece I use is bad, but it was a substitute that was driven by the impulse I wanted to destroy. For now, it is a product that I never recommend.
This review is about item#10009562.
Mainly processing of shutter etc.
1
From Japan
On 2009-06-20 22:04:18
I trusted it because it is a product of Mr. Bessel and I was disappointed when I tried using it because it is a pretty price. I think that it is unsuitable for people seeking work speed.
This review is about item#10009562.
Repair and remodeling of medium size motorcycle
4
From Japan
On 2008-11-16 00:51:35
It is much easier to use than the cheap rivetas I used before. Because there is a ratchet mechanism, the force per handful is small. However, because the head is large for the ratchet mechanism, it may be hard to use in a narrow place.
This review is about item#10009562.
1
Customer Who Viewed This Item Also Viewed
Doit Hand Riveters
Hand Riveters
Hand Rivet Set
Riveter Nutter
Hand Riveter Tool Kit
Hand Riveter, Ironwork
Hand Riveter
Flex Hand Riveter
LOBSTER Attachment Riveter
Hand Riveter
Power Riveter Attachment
Hand Riveter
Hand Riveter
Hand Riveter
Air Riveter