Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Construction Pencil 1.3mm

Construction Pencil 1.3mm
Sales Price: 5.99 SGD
Review Rating: 4.36
11 Customer Reviews
5 star 9
4 star 0
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Purchased for DIY.
5
From Japan
On 2017-08-15 12:43:48
Until now it was an ordinary sharpen, but the hardness is hard 1.3 mm 1.3 mm core is "moderate" as "snuff". This time I bought a red color, but I am also thinking of black color.
This review is about item#10034175.
Plumbing work
5
From Japan
On 2017-03-15 16:03:15
Even if it is attached to a helmet etc, it does not matter because it is thinner and lighter than magic to mark pipes cut etc. The core is also hard to break and very convenient to use.
This review is about item#10034166.
Basketball
5
From Japan
On 2015-10-24 20:42:58
Good to write.
This review is about item#10074732.
I bought it for woodworking black ink
1
From Japan
On 2015-06-17 23:12:53
I bought it for woodworking for inking, but it is 0.13 mm which is wrong unit, because the pencil size is similar to ordinary pencils, the 0.5 mm pencil pen is better
This review is about item#10034166.
Documents at customer's order
5
From Japan
On 2015-04-08 21:53:05
It is the same thing as replacement core, but it is very easy to use and employees are pleased. First of all, the core is thick and can not break, and it is easy to see even after writing.
This review is about item#10034166.
Used for woodworking postcards
5
From Japan
On 2014-04-22 21:57:54
Pencil and ballpoint pen up to now. Although I was injured in the magic, the pencil was clearly visible, but the tip ended tightly, it dropped and the tip was chipped and it was difficult to use, the ballpoint pen and the sharpening pen was difficult to see, the magic became useless immediately after the magic And none of them were good, but this product covered them well. Since it can also injure a metal object, it is also used for a workpiece that is not strict tolerance.
This review is about item#10034166.
It's a bastard!
5
From Japan
On 2014-03-31 19:52:03
A word of easy to use is exhausted!
This review is about item#10034166.
Smudge on metal · tree
2
From Japan
On 2013-05-20 23:52:23
· I can not write it well. · During the movement, the upper cap detached without permission and the spare core and cap disappeared. Should be a screw type cap.
This review is about item#10034175.
For sanitizing electrical work
5
From Japan
On 2013-04-09 09:22:19
As the people around me are told, it is exquisite thickness. I chose a consolidated core, but I am happy to write well and see the inking well.
This review is about item#36702382.
Inking at site (especially used for aluminum and iron)
5
From Japan
On 2011-05-23 13:15:50
Although it is a feature that it does not have to be scraped off, if you are using it for concrete etc, the tip will collapse and the core will be hard to come out.
This review is about item#10034166.
I am using it for writing. Ideal for writing notes without looking at hand. You can write without worrying about writing pressure.
5
From Japan
On 2009-12-11 11:38:04
I hope it is a bit thicker.
This review is about item#10074732.
1