Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of ALC Big Anchor

ALC Big Anchor
Sales Price: 12.99 SGD
Review Rating: 4.45
11 Customer Reviews
5 star 8
4 star 2
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
I ordered it with shipping on the day, but I was deceived. There is also a problem in correspondence after that! !
1
From Japan
On 2018-01-15 22:01:12
I ordered it with shipping on the day, but I was deceived. There is also a problem in correspondence after that! !
This review is about item#39303442.
Electrical construction
5
From Japan
On 2017-08-24 17:22:13
I am very satisfied. Inexpensive top. The strength is also perfect. rest assured.
This review is about item#39303451.
Installation of hardware
4
From Japan
On 2017-07-21 16:02:14
I think the goods themselves are good Attached stick stick is weak! Since you can break easily as you strike a hard line I hope the bars are made of metal rather than resin
This review is about item#39303424.
Piping support mounting
5
From Japan
On 2016-11-06 18:24:01
I purchased it because it was a size that I did not put much in the home center etc. It was saved.
This review is about item#10040606.
Renovation work of steel frame
5
From Japan
On 2016-08-02 18:34:04
This one item of usual! Stable quality.
This review is about item#10040606.
Temporary works
5
From Japan
On 2016-02-04 20:12:46
I purchased exactly the same thing from other stores at other shops, but by the way, it is cheap!
This review is about item#10040606.
Attaching the board to the ALC wall
4
From Japan
On 2015-11-07 20:06:47
If you are looking for M8, hit this item. It is very easy because it only punches with a prepared hole. Since we only need 11.5 mm pilot hole, we searched around drill bit, but we were able to confirm now that it is only made by company B so delivery takes about 4 ~ 5 days. Recommended for those who are not in a hurry but purchase a new concrete bit or already have a drill bit of 11.5 mm! One sticking rod is also attached with resin, but it is bent and it is short so it is hard to use. I constructed it with the tool of Company D. Since we also got a concrete bit of 11.5 mm this time, we will use this anchor next time.
This review is about item#39303424.
It is used for attaching items of about 5 kg or less to the wall of the ALC in the factory.
5
From Japan
On 2015-02-20 13:14:49
Although an anchor for ALC seems to be a lot of exaggerated things or a screw type screw-in type, I felt that many workers were unlikely to have workability. ALC pick anchor is very easy as it only needs to open a hole. However, since the jig for driving the attached pin is too soft, it is difficult to drive the pin, so a metal round bar (φ6.5 or so) was substituted. I fixed the thing, but it is fixed very firmly and I am very satisfied.
This review is about item#39303424.
Installation of box etc on ALC board
5
From Japan
On 2014-10-11 13:49:17
The price is low and workability is good.
This review is about item#39303424.
Scaffolding
5
From Japan
On 2014-03-12 14:50:28
It works well.
This review is about item#10040606.
Stopper bracket for wire drawing insulator.
5
From Japan
On 2012-04-13 10:26:21
There is considerable strength, you can use with confidence.
This review is about item#39303442.
1
Customer Who Viewed This Item Also Viewed
Hit Anchor
Female Screw Anchor
Wall Anchor Plug
Male Screw Anchor
AX Plug
Plug with drill
ALC Anchor Bolt
Blocker (ALC block for anchor)
Purakongu PC310
Np Alc Anchor Nba Type
Female Screw Anchor Trio
Hit nail
turbo
ALC female screw anchors
ALC male screw anchors
Wall Plug Anchor
Yale anchor
Fisher turbo anchor FTP
ALC Plar Anchor