Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Wheel, Rubber, With BWheel434 S-Fr

Wheel, Rubber, With BWheel434 S-Fr
Sales Price: 8.99 SGD
Review Rating: 4.33
6 Customer Reviews
5 star 2
4 star 4
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Repair of suitcase
4
From Japan
On 2018-03-03 13:02:44
I bought it because my suitcase caster got broken. Other than that, I did not have the original size diameter, but I found it easily on this site. The feeling I used was also durable and good
This review is about item#37972523.
For motorcycle maintenance stand wheel replacement
4
From Japan
On 2017-09-27 16:53:08
Three types of stands for maintenance of motorcycles are used, but even if they are well-known manufacturers with high prices, the wheels are made of resin, so they will not work due to aged deterioration. A large load is applied especially when lifting large vehicles, so the burden on resin wheels is great. Even though the metal part of the stand is firm, the tree type wheel becomes useless and it becomes useless. So I found the same size and width as a monotalou and diverted it. I can also lift a 200kg bike, but it can be used without problems.
This review is about item#35772432.
Maintenance of aluminum door
4
From Japan
On 2016-12-20 23:49:56
Movement is smooth and easy to use. I regret not having an explanation that takes more than two weeks to deliver
This review is about item#8163687.
Used for maintenance of dolly
5
From Japan
On 2016-09-20 18:19:53
I stacked up the containers and carried them, but because the car was supporting and the movement became dull, I exchanged it. The movement became smooth and became very easy. Until now I have purchased brackets but we purchased only the wheels this time, so we are thinking about exchanging other trolleys because it was cheap.
This review is about item#8163687.
Wheel change of dolly
4
From Japan
On 2015-05-14 13:06:56
There are many kinds even with the same size and the same manufacturer, and I do not know the difference at the same time. Every time I try to make a different type, I do not seem to have any trouble especially when using 3 to 4 years.
This review is about item#08163696.
Used as repair of carrier
5
From Japan
On 2014-01-20 01:05:54
I am satisfied that it seems to be stronger and last longer than the wheel before repair.
This review is about item#35772432.
1