Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Wheel, Elastomer, W/BWheel429E-Lb

Wheel, Elastomer, W/BWheel429E-Lb
Sales Price: 5.99 SGD
Review Rating: 4.91
11 Customer Reviews
5 star 10
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Carrier back caster wheel exchange
5
From Japan
On 2018-02-27 15:24:46
Since the width of the caster on the carrier back is narrow, is it dust-free? The wheel cap could not be installed. Steel pipe and needle bearing on the shaft, rolling resistance decreased.
This review is about item#8163617.
Caster bag repair
5
From Japan
On 2017-11-13 21:23:58
Basically it turns quietly, but depending on the position of the cover there is a slight rubbing sound You must to do something before you go on. There should be no problem in terms of use.
This review is about item#8163617.
As a supplementary part of a circulation car that the nurse always uses
5
From Japan
On 2017-05-18 14:59:27
Because it is always in use, the wheels that were worn at the time of purchase were exhausted, but it seems that exhaustion has decreased since it was replaced with this product.
This review is about item#8163644.
Wheel exchange for luggage
5
From Japan
On 2017-03-15 15:32:21
Since the wheel of the luggage attached from the beginning was unknown, it was broken if it was overworked with heavy luggage, so after exchanging, the reinforcement around the bearing, the exchange, product precision became smooth smoothly, load resistance seems to be good . It is likely to withstand vibration absorbing well even on foreign paved roads.
This review is about item#8163626.
Replacement of aged worn cart wheels
5
From Japan
On 2017-01-22 16:07:00
Although it is purchase additionally, I liked very much because the sound is quiet and movement is smooth.
This review is about item#8163644.
Carry back casters
5
From Japan
On 2016-10-21 10:08:18
Because the surface is soft, it is smooth and smooth even if it rotates because it contains rolling sounds and bearings. I like it. The rest is durable.
This review is about item#8163617.
Change suitcase caster
4
From Japan
On 2016-07-13 20:32:35
Originally I was looking for a 60mm bearings caster, but I installed a slightly processed suitcase side. Rotation is stable, smooth and satisfied than original caster. It was even better if there was 60 mm size.
This review is about item#08163626.
Used for in-hospital rounds
5
From Japan
On 2016-03-02 19:26:22
It exchanged due to aged deterioration. I thought that it would be quite expensive to ask the contractor and I replaced it myself. It will withstand full use if the dimensions match.
This review is about item#08163644.
Wheel change of dolly
5
From Japan
On 2014-07-04 13:18:17
Since the wheels of the dolly that we were using were damaged, we exchanged 4 wheels. Wheel that was attached before was loud and rough, but it became quiet after exchanging for this product. I think that it is durability · · · · · · · · · ·. Since the wheel is the life of the trolley, it can be used smoothly like a brand new by replacing it. It is the best to be quiet!
This review is about item#08163644.
Replacing the wheel with a more quiet wheel due to the wheel breakage of the carry bag
5
From Japan
On 2014-04-10 09:28:02
It is different from the shaft diameter of the wheel attached to the carry bag, but purchased for the purpose of being able to be used more lightly and quietly when used. Although I had a hard time exchanging, the elasticity of the elastomer was very comfortable, and I heard almost no sounds generated at the seams of a few steps, concrete tiles, etc., the impact on hands became very small Great satisfaction. Although it is a luxury item than the wheel which was originally attached to the bag, it can be said that it is far superior to the price difference.
This review is about item#08163635.
Nisshin (handbag) cart rack T6-88 as a spare tire
5
From Japan
On 2008-12-01 14:40:52
Movement is smooth and quiet! I think that it is a hybrid car
This review is about item#08163644.
1
Customer Who Viewed This Item Also Viewed
Wheel, Rubber One Wheel425 E-R
Wheel, Rubber Wheel
Wheel, Rubber Wheel425G, E, S-R
Wheel, Rubber Wheel425 S-R
Wheels, Urethane Cars439 G-Ur
Wheel, Rubber Wheel445 G-R
Wheel, Hard Rubber Wheel
Wheel, Urethane, W/BWheel439S-Ub
Wheel, Urethane Wheel439E-Ur
Rubber Wheel 434M-RB