Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of T Grip Hex Wrench No.6500-L

T Grip Hex Wrench No.6500-L
Sales Price: 6.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 2
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
For motorcycle maintenance
From Japan
On 2018-03-04 04:30:15
It is easy to grasp and easy to use · · ·. A white character of 3.0 mm disappeared right away. It's too bad though it included a nice logo. Other 2.5 mm 4.0 mm 5.0 mm 6.0 mm 8.0 mm is not disappearing at all. Could you exchange it when you send it?
This review is about item#10076717.
Use it when removing motorcycle engine guard.
From Japan
On 2017-02-15 09:24:40
In the Richit wrench, I was looking for a suitable tool that was difficult to work with. I could not find a good tool, but I purchased it because it seems easy to use. Although I have not used it yet, I think that the feel I took in hand is good, so I made this evaluation.
This review is about item#10076726.
When attaching climbing hold to the wall
From Japan
On 2016-03-25 22:06:21
It was easy to use and cheap.
This review is about item#10076726.
I bought it to remove the lid of the seat post with bicycle suspension.
From Japan
On 2014-12-12 22:22:43
In my case I purchased this item to remove the lid of the part containing the spring seat of the "FFR" suspension seat post and to maintain it. In the case of the suspension seat post, the inner spring expands when closing the lid, so it is necessary to rotate while pushing the lid, but this article pushes the lid of the seat post when using the part of the hexagonal bar which is beside the grip It is very easy to tighten while tightening, I am satisfied privately. Personally, I prefer a person who had a head of a long hexagonal bar as a ball point, but this point was one disappointment. Perhaps, I think that I will purchase a ball point thing when I next purchase.
This review is about item#10076726.
Customer Who Viewed This Item Also Viewed
P Handle Ball End Hex Key
T Form Hexagonal-Bar Wrench
ATL T Type Long Hexagonal-Bars Wrench
Grip Ball Point Hexagon Wrench
T Form Hexagonal-Bar Wrench
T-Handle Hex Wrench
Grip Hexagon Wrench
T-type twin-head hex wrench
Comfort grip T-handle hex wrench
T Grip Hex Wrench No.6500
(28461) grip
T-type hex wrench