Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of 12.7sq socket (12 angles) (millimeter)

12.7sq socket (12 angles) (millimeter)
Sales Price: 8.25 SGD
Review Rating: 4.25
8 Customer Reviews
5 star 5
4 star 1
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Tighten the head bolt of the motorcycle.
5
From Japan
On 2016-11-16 19:51:26
The accuracy is also sure, and you can also trust the management with the torque wrench.
This review is about item#7111894.
For screw detachment
4
From Japan
On 2016-10-31 20:41:18
I will give up if the thread collapses with KTC. It is a manufacturer of trust.
This review is about item#7111903.
Vehicle maintenance
5
From Japan
On 2016-09-30 23:19:44
I worried about 6 corners and 12 corners, but I chose 12 corners for ease of use
This review is about item#7111946.
Mechanical repair
5
From Japan
On 2016-04-02 11:32:03
Can be used for a long time with KTC's goods. It was a price that was not different from that of the home center so it would be nice if it became even cheaper.
This review is about item#07111587.
Maintenance work
2
From Japan
On 2015-11-05 20:26:14
I think that accuracy is good a little more.
This review is about item#07111693.
Used for cars, bicycle maintenance
5
From Japan
On 2015-02-04 22:04:33
Quality, comfortable feeling has also been improved certainly compared to what has been done. Work can now be done reliably.
This review is about item#07111754.
Maintenance of industrial engine
5
From Japan
On 2015-01-15 13:46:28
It is used for maintenance of industrial engine. In the engine of the car manufacturer, there are places where 12 - 17 mm and 12 - angle bolts are used. I will use it at that time. Since the 12 corner of the maker item is not placed in the home center etc., I used the 12-sided socket of the inexpensive box wrench set by us. This time, Monotaro says that there are 12 Kaku made by KTC and have purchased it. Since it is 12.7, it can be used for a torque wrench of 1800 N · m.
This review is about item#07111641.
Removing the hub nut of the rear wheel of the domestic bicycle
3
From Japan
On 2013-07-05 19:51:00
The rear wheel of the domestic bicycle can not come off unless it is 15 mm. I bought it although it is not usually used. It can be used normally.
This review is about item#07111727.
1
Customer Who Viewed This Item Also Viewed
Socket (12pt./entery 12.7mm)
Socket (6 angels)
Socket, 6 points
9.5sq socket (12 angles) (mm)
12.7sq12 Angle Socket
19.0sq. Socket
Deep socket (12 square)
9.5sq. extension bar
Impact Sockets, Electroless Nickel Plating
Ratchet handle
12.7sq. extension bar
Finger ratchet wrench set
12.7sq. Socket
12.7sq. socket