Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of No. 6 multiuse bit

No. 6 multiuse bit
Sales Price: 8.99 SGD
Review Rating: 3.60
10 Customer Reviews
5 star 4
4 star 2
3 star 2
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Drilling of structural timber
5
From Japan
On 2017-05-18 08:29:33
Compared to inexpensive ones, the bit of StarMem purchased because the sharpness lasts long.
This review is about item#10234655.
Fixtures
3
From Japan
On 2015-10-05 14:44:05
Normal upper class !!
This review is about item#10234655.
Drilling to pass electric wires
1
From Japan
On 2015-05-13 20:31:00
Applicable model: Since it was written as impact driver, I bought it, but I can not use it with impact. Regretting that I did not check the shaft diameter was regretted. I am using an electric drill without any help. Please do not write impact on compatible models.
This review is about item#36809123.
Drilling of a do-it-yourself carpenter
1
From Japan
On 2014-09-19 16:13:41
worst! It is! It is! I tried buying it because I believed the review (The review was not 3 mm in diameter?) When I opened 6 holes with a depth of 38 mm in 2 × 4 material, the top of the blade grew (the metal part of the spiral reached It became linear) and it ended. Driver worked at low speed using drill driver instead of impact. I felt 3 mm wood drill blade "necessary" in the first place I was immature. We will not purchase drill bits for woodworking less than 3 mm in diameter.
This review is about item#10234655.
Drilling
5
From Japan
On 2014-07-16 16:14:03
I am using sharpness for many years.
This review is about item#10234716.
Electric construction / drilling of wood
4
From Japan
On 2013-06-24 20:30:25
I wanted to use it with impact, but the axis was thick and I could not use it. Use it with electric drill or corner drill.
This review is about item#35723755.
To drill through the wire
3
From Japan
On 2013-02-15 12:49:00
I bought it for free shipping fee. I have not used it yet, but I think that it is not different from what I have used so far.
This review is about item#10234786.
For house wiring
5
From Japan
On 2012-10-17 13:45:01
Quality is also satisfied well.
This review is about item#10234917.
Used to drill holes through 3 boards
5
From Japan
On 2012-10-05 00:26:39
I used it in a drill machine, but I could punch a straight line without blurring.
This review is about item#10234831.
Drilling of battledore
4
From Japan
On 2012-07-05 18:23:41
Wood chips tend to clog the drill
This review is about item#10234856.
1
Customer Who Viewed This Item Also Viewed
No. 4 drill bit
Auger Bits,Long
No.1 short bits
No. 2 combined use bits
No. 5 short bit
No. 7 Impact Bit, Long
Brad Point Bit
Blacksmith
Combined bit
Combined Bit