Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of No.36 Adjustable Circle Cutter

No.36 Adjustable Circle Cutter
Sales Price: 48.99 SGD
Review Rating: 4.33
9 Customer Reviews
5 star 5
4 star 3
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Purchase to use a long bar
5
From Japan
On 2017-11-29 09:26:51
The more you are afraid of your teeth, the better you are. I strongly suggest that if you have long bar items from the beginning COSPA is good.
This review is about item#10236466.
Used for drilling work in indoor walls and doors ventilation holes and ventilation holes
4
From Japan
On 2016-04-04 20:38:27
It is reliable because you can open a hole of about 100 mm in diameter freely. A hole of about 50 mm was using a round hole saw, but it was impossible unless it was still a free cone again beyond that size. The use impression can be said to be "difficult". Getting used to it. A thin plate like a door needs to adjust the rotation speed, and fails unless it firmly fixes it. At present, the ventilation holes of the doors are beautifully finished and satisfied. that's all
This review is about item#10236466.
Speaker opening
4
From Japan
On 2015-12-13 12:33:03
It gets rampant until get used to. Fixing the board with a clamp is used to prevent injury. It is an item that needs to get used to. It is essential to practice with half-timed trees. There are figures in the manual but figures carved is a guide. But there is a precision of about 2 mm. Exact revision work will require trial cutting.
This review is about item#10236466.
To circular drilling of wood
5
From Japan
On 2015-09-07 22:56:45
Used for drilling of wood. The center easily opens a hole. I will cut the surroundings from there, but if I do not lower it vertically it will shake and shake. I am quite scared. There is cutting force, anything can be cut to plywood, veneer, plaques.
This review is about item#10236466.
Drilling downlight
5
From Japan
On 2014-10-05 16:13:47
Dedicated tool for downlight hole drilling is very expensive so it was nice to buy this! The gypsum board can be cut easily like paper.
This review is about item#10236466.
Processing wood
2
From Japan
On 2014-04-12 15:04:17
Usability is not as good as I thought It is not possible to adjust the length of the cone, again over and over
This review is about item#10236466.
Opening of floor board etc. in case of water supply / drainage construction
5
From Japan
On 2013-12-11 20:41:46
I hope the chuck part has variation with the hexagonal axis of the electric drill, the SDS bit, the impact axis
This review is about item#10236466.
Drilling in wood
5
From Japan
On 2013-11-05 11:33:54
Although I used it a lot, it is safe in the meantime, but there are no other things to change.
This review is about item#10236466.
Use small accessories (clock) to drill over 10 centimeters.
4
From Japan
On 2013-03-29 19:41:43
I fixed it to a tabletop drilling machine and worked fixed with holes, so I was able to punch holes very accurately. I could not make a big hole in Horseau, so I am very satisfied.
This review is about item#10236466.
1
Customer Who Viewed This Item Also Viewed
Universal Drill W
Free drill for metal work
Free hole saw
Universal Drill
Free drill M
Circle Cutter
Circle Cutter
FREE CONE SD
Woodworking Circle Cutter