Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Universal Drill W

Universal Drill W
Sales Price: 51.99 SGD
Review Rating: 3.44
9 Customer Reviews
5 star 4
4 star 1
3 star 1
2 star 1
1 star 2
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Cut disc from disc plate
5
From Japan
On 2017-05-27 15:02:08
I studied Holso and this free saw to make a disk shaped plate and made it free saw with price. I replaced it with a replacement blade for woodworking and cut it as beautifully as Holsaw if paying attention to the rotation speed and the vertical direction. Also, it is good that you can adjust the diameter freely.
This review is about item#10252627.
When creating the baffle of the speaker
4
From Japan
On 2016-10-06 07:02:42
Although there are also cheap ones of the same kind, this product was able to shave cleanly with a high ability to shave woodworks with firm making.
This review is about item#10252602.
Drilling work of wood
5
From Japan
On 2016-08-17 10:10:55
I was very satisfied. Is an optional item such as a cover for preventing chip scattering, it is still satisfactory.
This review is about item#10252602.
Steel material off
3
From Japan
On 2015-04-06 09:11:02
I pulled out the center drill and tried to cut the O type disk of the copper plate, but it was impossible. There seems to be a cone for O type disk cutting, so we will consider that. There seems to be only one type, so I think that you can increase the type.
This review is about item#10252627.
Drilling of wood etc.
2
From Japan
On 2012-12-04 08:55:00
As with the review below, black fixing hardware eventually broke both 2 as well. The first one was broken soon after purchasing, but I replaced it with the same old thing (white), but I thought that because the second one got broken, I was upset and I did not even sell this part alone After examining it, I understood that everyone was broken and posted it. We urge you to urgently perform material improvement and parts setup.
This review is about item#10252645.
Mainly drilling of wood
1
From Japan
On 2012-08-16 13:24:56
In the first use after purchase, a hole of 15 cm in diameter was opened in the control panel, and a conical part (black) between the screw and the bar broke and flew away in the middle of the second. It is neither a strongly closed translation nor an impossible force imposing during the drilling, so no point of intersection goes. Because there is a similar review, is it such a product?
This review is about item#10252602.
Hole opening with irregular size
5
From Japan
On 2012-08-15 01:24:22
A 215 mm plywood successfully entered a 02546187 parallel caster in a hole of 57.3 Φ. Because the horizontal axis was too long with the hand-held drill machine, I cut it and used it. Two blades were more stable than a single blade, and work was easy.
This review is about item#10252627.
Drilling of ceramic siding board
1
From Japan
On 2011-08-25 20:22:46
It broke in the second drilling after purchase. During the drilling, both of the rings for securing between the butterfly screw and the bar (in the picture, it looks whitish, but the one that arrived was a black ring) cracked , The fixation did not work, the surface of the ceramic siding became staggered. It is really frustrating. I thought "Return money!"
This review is about item#10252627.
Drilling of downlight, drilling of ventilator etc.
5
From Japan
On 2009-07-11 21:33:43
Since it can change the diameter with a butterfly screw instead of the conventional hex bolt, it is easy and good. Attention is necessary as it violates left and right at the moment the hole is opened.
This review is about item#10252602.
1