Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of No.26 Hexagonal Shaft Drill For Stainless Steel

No.26 Hexagonal Shaft Drill For Stainless Steel
Sales Price: 9.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 6
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Used for stainless steel angle drilling.
5
From Japan
On 2017-11-12 15:19:13
The hole was empty very smoothly. Even with an angle of 5 mm stain, holes were readily available. I will buy it again.
This review is about item#10252286.
Construction
1
From Japan
On 2016-10-20 17:46:08
We ordered around Monday night around 6 o'clock, so we shipped the item on the same day so we thought that it will be next Tuesday sending but we did not ship on Tuesday without any contact. Wednesday it was finally notified that the shipment was delayed and we will ship it today. I had to forgo the construction day by day, but there was a notification of the shipment delay again on Thursday today, and I heard that we will ship today. If you can not ship as planned, you should contact the venue in advance at least not on the next day you could not ship, but we are sorry late and we will ship today if you contact us, if there is further shipment delay from there It is impossible to do as a service for traders.
This review is about item#10252252.
SUS, iron drilling
5
From Japan
On 2016-04-12 20:55:32
Accuracy is good, it breaks well. Even wearing is OK. You can purchase with confidence.
This review is about item#10252146.
Used for drilling work
5
From Japan
On 2014-05-09 13:52:33
I'm very satisfied because the base and the base are firmer than the things I used to date.
This review is about item#10252191.
Used for iron stain
5
From Japan
On 2013-12-13 15:59:01
It is satisfying because it is sharp
This review is about item#10252252.
Drilling of metal
5
From Japan
On 2012-05-15 15:04:24
Although it will expire normally, since the price has been revised, "I will not continue purchasing". If you return to the price when you purchased it is "definitely recommended". We recommend drilling tool rather than impact. Impact is an instantaneous torque with a built-in striking with an anvil, but the torque itself is very weak. As a result, work efficiency is bad, as the tip gets bitten, a blow is added and a large force is instantaneously applied to the drill, so the tip is lacking. Sharpness also does not last long compared to drills with only rotation. In this size (thickness), I think that there is no problem first, but if it is the worst, the drill breaks.
This review is about item#10252347.
Drilling of stainless steel etc.
5
From Japan
On 2012-01-25 20:39:59
The price is reasonable, the sharpness is good, I can polish it, it is quite good Good things I do not want the price to change.
This review is about item#10252225.
1
Customer Who Viewed This Item Also Viewed
Spot Drill
No.20-E Hexagonal Shaft Drill For Iron Works
No. 20 Hexagon Shaft Ironwork Drill
Cobalt Drill
Hexagon-head axis puncturing
Drill Bit
Hex Drill Bit
Hex robe bit socket