Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of No.28-S Hexagonal Shaft Spiral Tap

No.28-S Hexagonal Shaft Spiral Tap
Sales Price: 13.99 SGD
Review Rating: 5.00
4 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Metal Processing
5
From Japan
On 2016-09-29 16:22:12
I tried using it variously, but I can be used with confidence and I am very saved. Thank you very much.
This review is about item#10252417.
Control panel production
5
From Japan
On 2016-04-05 15:02:57
I use it by removing the chips every time and attaching tap oil. I used about 60 pieces on 2.3 mm steel sheet, but it seems to be still alright.
This review is about item#10252417.
Pipe support material installation
5
From Japan
On 2015-07-29 21:51:52
When it is constructed with a typical tap with an impact driver, it will loosen and disengage from the chuck when it is returned, but since it can be mounted directly to the impact at 6.35, it can be constructed without any trouble.
This review is about item#10252426.
2.3 t New tap on steel plate or used for painted steel plate.
5
From Japan
On 2013-01-11 12:43:42
Because it is a hexagonal axis it can be easily applied with a charging screwdriver etc. It is very convenient. The use frequency is not so high, but it is not broken yet because it sticks.
This review is about item#10252426.
1
Customer Who Viewed This Item Also Viewed
No.28 Hexagonal Shaft Tap
Hex Shank Tapping Drill
Hexagon-head axis spiral fluted tap
Hex Shank Taps
Point Threading Tap
Hex Axis Drill Tap