Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of The Aluminum Sleeve for Nylon Covering Stainless Steel Wire Ropes

The Aluminum Sleeve for Nylon Covering Stainless Steel Wire Ropes
Sales Price: 6.83 SGD
Review Rating: 4.09
11 Customer Reviews
5 star 5
4 star 2
3 star 4
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Used to connect wires when self-making taco tentaya
5
From Japan
On 2017-07-03 16:58:39
I can fulfill the purpose by fitting the thickness of the wire firmly I am satisfied.
This review is about item#8344664.
Used as a fastener for anti-theft fixed wire of PC and USB memory
5
From Japan
On 2016-12-23 21:49:40
There is no collapse of the cross section, there are no individual variations and it is a beautiful item and there is no problem. Satisfied
This review is about item#8344664.
Wire gauze
3
From Japan
On 2016-05-23 20:10:22
Functionally it is not particularly good or bad. I wish it would be a little cheaper because the cost is high ,,,
This review is about item#10263093.
Used for electric chain block (for movement of chain block)
3
From Japan
On 2016-03-30 19:34:42
usually
This review is about item#10263093.
work
3
From Japan
On 2014-11-27 15:38:15
I should have bought a little smaller, I failed. I thought it would have been better if I could make it look like an actual size image.
This review is about item#08344673.
Loop making of wire for preventing falling of furniture
4
From Japan
On 2014-06-03 19:21:49
Since it was a nylon-coated wire, I bought a sleeve for nylon coating. I think that it depends on the caulking machine, but I tried pulling the nylon-coated wires of 2.0 mm in outer diameter exactly with human power, but naturally it did not bother me. For applications that prevent furniture falls, it is sufficient in terms of strength, and if you think of the same use, I think that it may be smaller one size.
This review is about item#08344673.
Used for wire connection
4
From Japan
On 2014-03-24 18:22:14
Measuring instrument screw is connected by wire and used. It is very useful.
This review is about item#08344673.
Wire binding operation
3
From Japan
On 2014-03-17 06:12:32
It is the best impression that the price is cheap The commodity itself is not so different from others
This review is about item#08344664.
Aluminum sleeve for nylon-coated stainless steel wire rope
5
From Japan
On 2013-09-06 13:19:36
I packed the paper all over in a big box and sent it. There are more paper. Just like the Amazon, tape on the bottom, paste it.
This review is about item#08344664.
Wire binding
5
From Japan
On 2013-06-02 00:19:42
It is the same as what is in the home center. The entry of 20 pieces is very convenient. @ If you have a long sleeve you want to buy.
This review is about item#08344664.
Bundle of nylon coating wire
5
From Japan
On 2013-05-25 23:56:24
It is the same as thing which sells to home center etc. It's cheap price and 20 pieces of convenience
This review is about item#08344664.
1
Customer Who Viewed This Item Also Viewed
Arm crimp plier
Wire Rope Sleeve
Arm Oval Sleeve, Aluminum
Stainless Steel Wire Rope
Aluminum Sleeve
Clamp Cutter
Aluminum Clamp Pipe
Circular Sleeve
Oval Sleeve
Stainless Wire Rope Bobbin
Wire Clamp Plier
Wire Clamp Plier