Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Acrylic Level, Flat Type

Acrylic Level, Flat Type
Sales Price: 12.99 SGD
Review Rating: 3.33
3 Customer Reviews
5 star 0
4 star 1
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Piping Preheating is the best.
From Japan
On 2017-04-21 19:05:16
Compact and easy to carry around. It is easy to see, not crazy. Useful for the use of narrow parts.
This review is about item#10085311.
LCD monitor and digital camera
From Japan
On 2016-03-14 11:22:09
I am using the liquid crystal wide monitor after setting it to 24 inches (1920 × 1200). Since there are a lot of drafting relationships with the monitor installation, the inclination is anxious. Since the level is light, it is affixed with double-sided tape on the top of the monitor. It is clean and very beautiful because it is made of acrylic. In vertical writing etc, especially the inclination of the letter is concerned, the neck will tilt, the direction of the stiff shoulders may be better. My digital camera is old, so I have no level. When shooting site photos in the mountains, you will not understand the horizontal sense, so use it at that time. I shoot it with a digital camera next to it, but it will not work if there are protrusions of a digital camera.
This review is about item#10085311.
In-house can making work
From Japan
On 2013-12-16 13:36:00
I have not used enough to write comments yet, but I feel just fine in terms of size. Although it is a type without magnets, it is using a magnetic sheet pasted.
This review is about item#10085311.
Customer Who Viewed This Item Also Viewed
Aluminum Level
Carpenter's Square Level PS-70
Pocket Slope Meter
Level Guage With Flat Eye Bell Magnet
Designer's Compact Level
Aluminum Level
Handy Level Light
Pocket Level
Handy Level
Mini Level
Bubble Level
Mini Level Revo
Transparent Level
Kurutoga with rubber grip