Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Code Cover, Soft, Mound Type

Code Cover, Soft, Mound Type
Sales Price: 10.99 SGD
Review Rating: 4.12
8 Customer Reviews
5 star 4
4 star 2
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Protection and consolidation of floor cables
4
From Japan
On 2017-11-17 01:04:18
There is no particular problem except for the color that I thought was different. It is so soft that it does not hurt even if you step on it. Somewhat lower and a little lower
This review is about item#10751291.
Bundle the cables on the floor
4
From Japan
On 2017-10-31 04:37:25
So soft so it is gentle to the foot when stepping on. Because it has a shape like a camouflage, it will catch when the chair goes through. It might be a good shape if the supreme like Mt. Fuji is spread out. Because it sells in a rolled state, it suffers from its habit, it struggles when sticking to the floor, and it is easy to peel off. In fact it seems that there was no need for a 3 m roll.
This review is about item#10751237.
It covers the wiring code of the exhibition.
5
From Japan
On 2017-10-22 13:04:03
We use it to avoid the danger of wiring cords at the exhibition that welcomes many customers.
This review is about item#10751167.
For demonstration (indoor electrical wiring)
3
From Japan
On 2017-09-21 10:50:06
It is very easy to use and it is the second order. Thank you for considering the price.
This review is about item#10751133.
In the office
5
From Japan
On 2016-07-07 08:43:50
If you use software you may not be able to use hard. It is good not to break.
This review is about item#10751176.
PC HIMD wiring protection from projector at small hall
2
From Japan
On 2016-02-08 11:02:02
Since those of 2 m are rolled up and packed, the curling habit can not be taken quite easily, both ends become arched and float up, and the role of flat mall can not be fulfilled. It was necessary to add such as sticking with a curing tape. The one in 1 meter was in a straight state and it was not a problem to use immediately.
This review is about item#10751194.
Event cabling
5
From Japan
On 2015-07-16 15:18:05
It was light and the work was done quickly. It was strong.
This review is about item#10751273.
For cable wiring at events
5
From Japan
On 2015-07-16 15:16:22
Very light and easy to use. I was able to work immediately.
This review is about item#10751273.
1
Customer Who Viewed This Item Also Viewed
Cable Protector
Cord Protector
Ud Protector
Cable Protector Soft Type
Cable Protector, 20mm Cable
Soft Color Protector
Cable Protector
Cable Protector
Flat Cord Protector
Cord Protector
Cable Protector
Floor Cord Cover
Cable Covers
Guard Man IIR
PVC Protector