Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Plywood Screw

Plywood Screw
Sales Price: 15.99 SGD
Review Rating: 4.25
4 Customer Reviews
5 star 2
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Fixing the sheathing board and the sacrificial board
5
From Japan
On 2018-03-02 01:10:06
Usually I think to hit a rain or the like with a courtlet etc, but sometimes due to the screw under the neck, the rafters and floats rise to the rafters may cause trouble afterwards. However, this is only an exclusive item, it is understood by seeing under the neck, but there is no screw unnecessary by the amount of control. Besides, with flexibility, it becomes flush, exactly cheap, and it is the best cost performance. ※ Although it was said that the Bali comes out in the review of the other person, since this screw is not a screw for the purpose of finishing as it is in the first place, to use it to worry about Paris which comes out somewhat, putty is put on it and finished with paper It is necessary to do.
This review is about item#10922642.
Floor covering base
4
From Japan
On 2017-07-05 12:17:29
I use it when hitting the control basement Bali will come out. Workability is good
This review is about item#10922667.
For fixing the control panel
3
From Japan
On 2015-11-25 15:30:17
usually
This review is about item#10922651.
Stop throwing plywood
5
From Japan
On 2013-10-12 21:08:35
The remodeling of the old house is optimal for stopping the floor sounding The burden of the control fee is small and construction of the finishing material is easy
This review is about item#10922642.
1
Customer Who Viewed This Item Also Viewed
Slim Threads
Course Thread
Particle Board Screw
Compagnis Parker
Konpanebisu Disugo
Fine Screw
Confit
End Check Prevention Screw
Compainvis (small box)