Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of New Carpentry Major

New Carpentry Major
Sales Price: 24.99 SGD
Review Rating: 4.00
3 Customer Reviews
5 star 0
4 star 3
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Dimensioning of wire material
From Japan
On 2018-01-18 09:10:39
It can be used even in machined oil spots and the scale will not disappear. Just cut the strap part because it passes directly through the metal part.
This review is about item#11131111.
Measurement in various scenes
From Japan
On 2018-01-04 23:30:24
It's compact, not rugged, fresh designs are good. It is also helpful to have a mechanism to loosen the shock in the mouth of the measure. The tension of the major was slightly weak, and I felt it was easy to break when stretched out.
This review is about item#11131127.
To a carpentry carpenter
From Japan
On 2013-02-11 21:54:48
Perhaps this should be the smallest in a 25 mm wide 5.5 m conveyor. I am very familiar with my hands and I do not yet find a good use impression than this. Although I purchased it several times and kept using it, I had to renew with the same symptom every time, and it was almost the life span of the site. A guide-like thing like a cushioning material between the nail and the main body comes into play while using it. It began to rattle soon, it got broken soon. When it disappears it is difficult to draw out and it gets hard to store. I am very sorry just because it was a good size conveyor.
This review is about item#11131136.
Customer Who Viewed This Item Also Viewed
Measuring Tape,
Measuring Tape, Stainless Steel
Measuring Tape, Stainless Steel
Measure Tape Loack Plus 19
Tape Measure
Magnesium Merasure Tape
Convex GOKUSHOH Cyclone
Convex GG EVO 19mm
Convex Waza Ari