Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Earthquake-Proof Halogen Type Floodlight

Earthquake-Proof Halogen Type Floodlight
Sales Price: -
Review Rating: 4.60
10 Customer Reviews
5 star 6
4 star 4
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Under the floor, behind the ceiling etc.
4
From Japan
On 2016-09-29 17:26:54
Since it is the purchase of the first lighting fixture, it felt purchased furiously. Since brightness can be adjusted, it seems that you can use it without difficulty.
This review is about item#11108307.
Lighting in climbing gym
5
From Japan
On 2016-04-13 16:59:19
Very bright, it is convenient to adjust the illuminance. It may be warm in winter, but summer may be hot.
This review is about item#11108307.
Candy work
5
From Japan
On 2016-04-10 18:20:55
It was written that it can be used for candy work for review, so I bought it. I have not used it yet, but I thought that it was expensive so I could not buy it because it is exclusive, I am looking forward to using it
This review is about item#11108307.
The workplace is dark and the hand is used for lighting for machining
5
From Japan
On 2016-03-05 21:14:23
It's easy to carry, and it's also cheap and bright.
This review is about item#11108307.
Shadowy lighting
4
From Japan
On 2014-02-19 23:01:52
Two years passed since purchase. After all, I was using illumination for 1 hour / day, but the result valve could be used without replacing it, but the dimming volume became poor contact and it became unusable. Due to the nature of the dimming circuit, I can understand the use of VR with SW, but is the reliability of parts? is. However, he worked hard for two years.
This review is about item#11108307.
Night work
5
From Japan
On 2013-04-17 14:48:11
I am active in various situations. Easy to use because it is convenient and compact as it can be placed on the floor or hung on the wall.
This review is about item#11108307.
Shadowy lighting
5
From Japan
On 2012-07-18 22:43:20
Since it used about half a year after purchase, it is an additional review. Although it is about 1 hour / day use, the attached bulb is not yet cut because I am using the illuminance dropped. Although I do not have a 500 w valve all the time, I think that it is good with a dimmer as well. I use it considerably lightly because it makes it to 250 w or less illuminance. Even a 250 watt projector does not have half a year, so I think it is economical as well. It is recommended for those who use 250 w type. It is slightly big.
This review is about item#11108307.
I tried using it as a lamp of candy work.
4
From Japan
On 2012-04-29 23:59:29
Since it is earthquake-resistant dimming type, it is good if it can be adjusted to subtle light adjustment. I can not buy a candy lamp at this price first, and the replacement bulb is also cheap so it is very helpful. Improvement may cost you money, so it is good to have attached clips.
This review is about item#11108307.
Work in a dark building or work in the evening
4
From Japan
On 2012-02-29 22:25:42
First of all, from the packing at the time of purchase, screws are stupid and can not be tightened The length is also different and also made in China! I thought about returning, but I used it because I want to use it in the work inside the building with rain the next day. I think that illuminance control is also appropriate for power saving by proper use between daytime and evening.
This review is about item#11108307.
Shadowy lighting
5
From Japan
On 2012-01-28 15:11:23
The usual emitter was very uneconomical because the valve was cut off quickly. Therefore, I thought about attaching the dimmer by myself, I knew this product and purchased it again. Do not use with 500 W full power, if you use it with reduced illuminance, the life of the valve has increased considerably. As for the brightness, it is especially good for those who use the 250 W type. 500 W type is large, so it would be good if there is a 250 W type.
This review is about item#11108307.
1