Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of 3 Sizes Tube Bender, Millimetre Type

3 Sizes Tube Bender, Millimetre Type
Sales Price: -
Review Rating: 3.88
8 Customer Reviews
5 star 3
4 star 3
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Used for bending copper clad pipe
4
From Japan
On 2017-06-21 16:55:16
It is useful when constructing a copper pipe in a place where R is small and narrow.
This review is about item#8742815.
Bending of copper pipes
4
From Japan
On 2015-10-24 10:51:44
Easily bent
This review is about item#08742815.
Used for bending copper pipe
4
From Japan
On 2015-03-10 18:59:30
I used it for bending the control tube 8 mm (clothing 1 mm), but it was able to be used without problems. Depending on the location, it's small, so I am happy to use it even in a small space.
This review is about item#08742815.
Aluminum pipe work
5
From Japan
On 2014-05-30 21:32:41
It bends easily and more beautifully. R Since the radius is fixed, it can be bent only by the fixed R, but it is appreciated because its use frequency is very high.
This review is about item#08742815.
Bend a pipe
1
From Japan
On 2014-04-05 13:48:32
Even if I tried to bend the pipe many times how to use it was broken pipe was bent at the part which was not used. I think that it is not made in Japan, but it is quite inconvenient because there is no such thing as an instruction manual in the box. I regret purchasing it.
This review is about item#08742815.
In kerosene piping etc.
5
From Japan
On 2012-10-22 23:09:22
Bending with minimum radius was easy to work smoothly.
This review is about item#08742815.
Bending of aluminum rods and stainless steel pipes
5
From Japan
On 2011-11-22 12:32:16
I thought that it would not be possible to bend a stainless steel pipe, but I could bend it easily.
This review is about item#08742815.
Aluminum tube bending process.
3
From Japan
On 2009-02-05 08:37:19
Outer diameter · 10 mm, wall thickness 0.8 mm can be bent to nearly 90 degrees. For the handle to bend this tube, the length is slightly short. I want +50 mm more.
This review is about item#08742815.
1
Customer Who Viewed This Item Also Viewed
Tube Bender
Tube Bender, Lever Type
Strong Tube Bender, For Stainless Steel - Copper T
4 Head Tube Bender
Lever type Tube Bender
3 Size Bender
3 Head Tube Bender
3in1 Tube Bender
Tube Bender
Color Tube Bender
Lever type tube vendor