Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Air Filter Separated Type

Air Filter Separated Type
Sales Price: 28.99 SGD
Review Rating: 4.00
10 Customer Reviews
5 star 4
4 star 4
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
For air piping repair
3
From Japan
On 2017-04-01 09:25:02
It looks like a small toy. It can only be used for terminal piping and the like.
This review is about item#2098415.
Air tool work
1
From Japan
On 2017-03-19 23:56:41
Purchased one year ago, it will not be usable anyway but after one year it is finally removed and discarded. Water is coming out from the tool if it is used for 15 minutes instead of continuous operation. Slightly water is accumulated, so it seems to be working slightly, but this is equivalent to garbage which does not endure at all in use. I can often sell it by making such a level. I thought that it could be used at the time of painting but I bought it, but when I use it for painting it will be ridiculous. . Even though it is cheap, it is a level that can not be sold!
This review is about item#2098415.
Repair of instruments
5
From Japan
On 2017-01-20 17:47:37
It is used for repairing the nebulizer instrument. There was a part number and it was able to be installed without any problem.Similarly it was something that the equipment maker does not have it.
This review is about item#2098415.
Compressor air filter
4
From Japan
On 2016-02-25 21:21:07
Installed between compressor and subtank. I catch water enough to be interested. I'm sorry that it's not perfect. Is it difficult to use it alone for painting? It is excellent from the point that it is inexpensive and compact.
Air Compressor
5
From Japan
On 2016-01-26 19:40:37
Used to remove moisture from air compressor. Use it because the machine freezes at the air outlet with air with high moisture when cooled to around 0 ℃. Machine store says it is said to be 5000 yen and purchase here was cheap and it was completely the same goods.
This review is about item#02098415.
I want to connect clean air between the compressor and the air gun
4
From Japan
On 2015-12-17 15:15:25
Because it is a proper manufacturer, it can be used with confidence, because it is unpleasant to buy cheap and buy again.
This review is about item#02098415.
Dehumidification of color selection air
4
From Japan
On 2013-04-09 06:34:16
The function removes the moisture corresponding to the price. I think that it is easy to put down if there is a direction sign on the main body that the manual is not written.
This review is about item#02098415.
Painting industry
5
From Japan
On 2012-07-16 17:55:00
It is satisfying because it will take the rough water. I am surprised at making good from the price. The drain valve is also different so you can replace it and you can use it for a long time. If the effect falls, it can be replaced immediately because it is cheap.
This review is about item#02098415.
Air drain
5
From Japan
On 2012-06-28 13:07:03
With this price this performance is reasonably satisfying. I am also solid making.
This review is about item#02098415.
Removal of moisture from the compressor
4
From Japan
On 2011-02-08 00:05:21
You can get good moisture by price. I make it well and it is made precisely.
This review is about item#02098415.
1
Customer Who Viewed This Item Also Viewed
Mini Air Filter
Air filter (Selex)
Air Filter
Air Filter, Large
Air Filter
Air Filter
Air Filter
Air Filter
Air Filter
Air Filter
Air Filter
Air Filter