Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pliers Wrench

Pliers Wrench
Sales Price: 109.99 SGD
Review Rating: 4.57
7 Customer Reviews
5 star 6
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
There are places to sell cheaper
2
From Japan
On 2018-03-08 22:56:59
There are places that sell cheaply through online shopping on the same item. It is a good product, you want it cheap a bit. After looking it up, you should buy it.
This review is about item#19070914.
Installation of cable gland
5
From Japan
On 2017-11-30 09:06:51
I continued to purchase 125 mm similarly. Since the cutting edge is flat, it can not be scratched and the torque can be applied sufficiently to the thing which it holds. Size adjustment requires separation, but I think that it will be impossible to leave if you become familiar.
This review is about item#32606104.
Bolt nut tightening, iron plate bending etc.
5
From Japan
On 2017-02-20 20:24:22
I bought it from a plunger wrench of a little old Kunipex. Although the feeling of operation was a smooth feeling of the old guy, it is handy because it is a wrench that can be used considerably. Besides fastening bolt nuts I like it because it is versatile as it bends, clamps or holds the iron plate.
This review is about item#32606104.
Grips such as plated parts that you do not want to hurt
5
From Japan
On 2016-08-03 22:10:40
Since the jagged portion of the slip is not processed, it can not be scratched though it can be grasped firmly.
This review is about item#32606095.
For nut turning
5
From Japan
On 2015-10-14 15:43:06
Easy to use
This review is about item#32606095.
Temporary fixation of equipment
5
From Japan
On 2012-11-23 15:10:00
It is written as "Non-ferrous metal nut, ideal for bolt" because it will scratch the note as it will not be used for nonferrous metals etc. It may be that it is self-responsible, but if you use carefully, you can turn make-up nuts etc. without hurting. Since it is possible to "grasp" objects of 0 to 60 mm in one size, the monkey wrench has been kicked out of the tool box because it can be rotated without damaging the screws than the monkey wrench.
This review is about item#32606113.
Machine alignment It was used when loosening the nut of 8 to 13 mm at the time of temporary assembly No force was applied in the direction to be opened at the time of turning and it was able to loosen as "sledi" without touching the contact surface without scratches Very easy to use
5
From Japan
On 2010-08-30 18:18:23
I think that it will be easier to determine the position if there is a mark like a monkey with memory
This review is about item#32606104.
1
Customer Who Viewed This Item Also Viewed
Cobra Water Pump Pliers
Control cabinet key
300mm pliers wrench
180mm pliers wrench
250mm pliers wrench
Cobra Water Pump Pliers
Mechanic Pliers
Pliers set Cobra set
Universal key