Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Diamond Bur 6mm Shank

Diamond Bur 6mm Shank
Sales Price: 18.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 5
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Processing of hobbies
5
From Japan
On 2018-02-01 21:34:43
Anyway get better. It is useful because it is easy to handle with a length just right for the wavelength.
This review is about item#32606271.
Machine repair, metal processing etc.
5
From Japan
On 2017-03-01 15:13:45
It is cheap and I am grateful. It is saved when there are products of various shapes like products of other companies.
This review is about item#32606271.
Maintenance of motorcycle
4
From Japan
On 2017-02-27 16:00:01
It was used to sharpen the piston pin. Although the pin is very hard, it could be cut without problem for diamonds. The angle was also well-tapered.
This review is about item#32606305.
Cutting inside the engine of the motorcycle
5
From Japan
On 2015-11-19 21:11:40
I really wanted a cone shaped diamond bar, but at this price it only had a spherical shape and I purchased it without any help. Regarding the use, it is not a problem to shave. However, it is enough to devise how to cut, but it is helpful if there is something conical and inexpensive, if possible.
This review is about item#32606271.
Polishing of aluminum.
5
From Japan
On 2015-02-22 14:49:11
My eyes are fine, so I feel like clogging, but I can crunch the cheeks apart from it. Very, workability is good. I think the price is also cheap.
This review is about item#32606271.
Detailed processing of stained glass
5
From Japan
On 2011-02-25 19:32:00
Obtained a long-awaited 6 mm shaft diamond bar (6 mm shaft has few products). Immediately attached to the router, trial running, big shake occurred. After several trial and error, finally I inquired to MonotaRo, there was a direct contact from the manufacturer. As a result of testing by the manufacturer, it is not a problem of the product, the overhang is too large (the overhang becomes 55 mm because the axis enters only about 25 mm in the router), the performance could not be demonstrated It turned out to be the cause. Carefully taught us how to use the product, we bother offering materials. I talked about various things, I decided to take measures to cut the axis and reduce the overhang, and cut it by 50 mm (by oversize) (overhang was 5 mm), it got no shake at all. Thanks to the manufacturer who kindly responded to the amateur without having trouble! is. From now on, I would like to use the company's products.
This review is about item#32606323.
We are using it for port machining of internal combustion machines and removal of aluminum edges and burrs.
4
From Japan
On 2010-11-16 19:49:47
I think that it is suitable for actual work if I get R to be gentle more gradually.
This review is about item#32606271.
1
Customer Who Viewed This Item Also Viewed
Electroplated Grindstone  EP Bar CBN
Electrocoat Diamond Bur
Diamond Bur, 6mm Shank
Diamond Bur
Electrocoat Shank E-P Bur DIA
Diamond Bur Spherical
Diamond Burr Bullet-type
Carbide Bar-sphere