Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Oil Pot Window, Permanent Type

Oil Pot Window, Permanent Type
Sales Price: 4.99 SGD
Review Rating: 3.50
2 Customer Reviews
5 star 1
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Machine maintenance
2
From Japan
On 2017-03-23 12:51:46
After replacing the oil pot the oil leaked out. Recently, there are many variations ,,,
This review is about item#2040096.
As trochoid pump operation confirmation window of second-hand lathe
5
From Japan
On 2017-02-04 14:43:31
Used lathe Others The window of a machine with a gearbox is almost black and it is not possible to check the flow of oil and oil so replace it with a new one. Perhaps the gear oil was oxidized and turned black, it was probably using it as nonteent. This time it is used to replace the window to check if the oil is properly flowing from the trochoid pump to the tube. Because it is a thing to confirm that the tube sticks in the middle and the oil stains from there, puncture a hole larger than 0.5 mm from the tube in the center. Open the hole with a small diameter with pin vise and then finish it with a thick drill. Otherwise the drill will inadvertently hit the inside of a clear window of acrylic (?) When the drill penetrates and it gets scratched and makes it unsightly. The most difficult thing was to remove the remains of Kiriko remained inside the window when penetrating and to insert the holes of the tube and the window when inserting into the machine. If this is a machine that can open the top cover of the gearbox, it is good to pinch the interfering tubes with the fingers from the inside of the gearbox. If it's an old machine (Hamatsu lathe or something else) the hole in the machine body may be bigger than Bimmy so at that time the oil sheet is wrapped around the side of the window, the old window gauge is standardized by another manufacturer (Takara etc) When it is totally different several millimeters, insert it so as to close the gap with epoxy putty for water leakage
This review is about item#2040096.
1
Customer Who Viewed This Item Also Viewed
Oil Pot Window, Permanent Type
Oil Pot Window, Permanent Type
Oil Pot Window, Permanent Type
Oil Pot Window, Permanent Type
Oil Plug, Pusher-Type
Oil Pot Window, Permanent Type
Oil pot window round type
Oil Pot Window, Permanent Type
Oil pot window HL type
Line type window
V-type (implant type)
Oil Level Indicator