Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Tight Anchor, Stainless Steel

Tight Anchor, Stainless Steel
Sales Price: 56.99 SGD
Review Rating: 4.50
12 Customer Reviews
5 star 9
4 star 0
3 star 3
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Mounting of wooden frame
3
From Japan
On 2015-05-31 15:40:38
Good
This review is about item#32631654.
Stainless steel cover fixing operation
5
From Japan
On 2014-10-27 07:12:04
It was very useful without problem for all work
This review is about item#32631645.
As earthquake resistant fixation of equipment.
5
From Japan
On 2014-07-29 17:55:45
Even compared with other manufacturers, there is not any change. Price should be cheaper. I want you to make an effort.
This review is about item#32631672.
Fence foundation to concrete
5
From Japan
On 2013-06-17 23:07:55
It was a certain product. I think that the quality is good.
This review is about item#32631715.
Fixing the handrail etc.
3
From Japan
On 2013-04-16 09:45:27
It gets stuck firmly as usual.
This review is about item#32631663.
Fixing outdoor lightweight items
5
From Japan
On 2013-03-16 08:12:58
I think that the feeling of use is good although it is used to fix the oil tank and fix the angle etc. Since size and length are changed for each weight, there is nothing to remember such as a problem in particular so far. Stainless steel is expensive when you buy it with decimal as there are places which are not put in tool shops and material shops etc. It is very much appreciated that this price can be bought at this price.
This review is about item#32631663.
Installation of enefme
3
From Japan
On 2013-01-21 17:56:26
I bought it because the price is cheap, but if it tightens too much, the nut may not become loose.
This review is about item#32631706.
Used to attach the stay to the concrete retaining wall.
5
From Japan
On 2013-01-13 20:46:22
Is pleased.
This review is about item#32631663.
To install laboratory equipment to concrete.
5
From Japan
On 2012-12-13 13:26:59
It was not different from the home center etc. I usually purchased.
This review is about item#32631672.
Electrical construction
5
From Japan
On 2012-08-23 10:10:15
There is no problem in use at all. However, the nut and the washer were separate. The nut size is also 17. (Sc-3060) Even this price is satisfactory.
This review is about item#35775047.
Equipment construction, for equipment fixation.
5
From Japan
On 2012-07-02 12:29:04
There is no problem in quality. I am satisfied with this price.
This review is about item#32631706.
Ground / Equipment installation etc.
5
From Japan
On 2012-01-22 16:02:02
I think that it is cheap compared with products of other companies and I think that there is no special difference. I would like to order this next.
This review is about item#32631663.
1
Customer Who Viewed This Item Also Viewed
Tight Anchor C Type
Stainless Screw Anchor
Tight Anchor Stainless Steel
Sleeve-All Anchor
SNSS-RY hexagon socket head bolts (Raydent processing)
Anchor C Type Steel
Tight Anchor, Hot Dip Galvanizing
All Anchor, Steel, Pack Product
Sleeve-All Anchor SC
Flexible Pipe for Water