Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stainless Steel Rotation Grip

Stainless Steel Rotation Grip
Sales Price: 10.99 SGD
Review Rating: 5.00
5 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Used for Hitachi drill D 10 VH
5
From Japan
On 2017-07-21 09:02:27
According to title I used it for Hitachi drill D 10 VH M10 The cheap Makita drill got broken soon It was a thing of Hitachi. Very horsepower is strong, work progresses swiftly and speedily There is horsepower, but on the top, the rebound to the wrist is also strong It's a merit but it's also a demerit So I found a genuine side grip But as this thing came out in relation I ordered the screw diameter and ordered it This is cool, it looks like it will last for a long time The gripping part rotates very good! ! ! I also thought I was going to get in the way when I fasted the screws It will be ok if you get used to it. Because it reduces the burden on the wrist all at once Fatigue overwhelmingly improved even if you shoot a screw for a long time Ideal for D10 VH users! If other drills were to be done to a certain extent I think that there is a mounting screw hole beside it How about installing it? By the way, because there were screw holes on the left and right It seems that you can also attach left-handed people
This review is about item#32721236.
Electric drill side handle
5
From Japan
On 2017-03-16 22:07:17
It was used as a side handle of electric drill (HITACHI D 10 VH). The length of the screw part (M 10) was also perfect, and it was able to be installed in a cool way as a genuine product without fine workmanship. With the feeling that some drilling work was carried out there was no particular problem, the work became easier because it can hold the electric drill securely with both hands. It may be my preference whether fixed type or rotary type is good, but in my case, it was a correct answer by selecting rotary type. As a request, I thought it would be nice if I had full length options.
This review is about item#32721236.
Replacement of machine adjustment handle knob
5
From Japan
On 2014-04-25 16:55:34
This is fantastic. Working accuracy is also good and it moves very smoothly. It was a cheap plastic version made before, so it feels extra well (laugh) Nothing to say if the handful is a little bigger.
This review is about item#32721236.
I am using it for ship's rudder
5
From Japan
On 2011-11-08 04:46:52
It's a little longer if you can, I'm happy if you have a big size.
This review is about item#32721236.
For small desktop lathe feed handle
5
From Japan
On 2011-03-10 18:35:47
This time, I bought it as a handle of a tool delivery table of a small desktop lathe. The STD does not rotate the axis, and the thing that the fingertip hurts with friction when working is also good ... This handle has no inconvenience for the rotary type, so you can work comfortably. It was good to purchase.
This review is about item#32721202.
1
Customer Who Viewed This Item Also Viewed
Stainless Steel Fixed Grip
Steel Rotation Grip
Rotating Grip
Handle Grip, Rotation TypeResin
Rotating Grip
Handle Grip, Rotary Type
Rotating Grip PP
Fixed Grip
Mini stainless rotation grip MSSR
Rotary grip RG
Stainless steel cylinder type rotary grip SSR