Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Uniball Signo Click Type Ultra Fine Refill

Uniball Signo Click Type Ultra Fine Refill
Sales Price: 0.99 SGD
Review Rating: 4.57
7 Customer Reviews
5 star 5
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Office equipment
5
From Japan
On 2018-04-11 16:34:57
It is used for office work together with red for many years. It is economical and satisfied because it can be run with almost a replacement core.
This review is about item#32906334.
Fill in the business diary
3
From Japan
On 2016-03-26 11:07:45
In the past, it was good because I thought that I purchased a ballpoint pen on the main body and I waste it. It's cheap!
This review is about item#32906334.
Delivery address of delivery
5
From Japan
On 2015-12-07 15:21:52
It is very easy to use because it can be drawn with light touch.
This review is about item#32906334.
Replacement core of ballpoint pen
5
From Japan
On 2015-06-18 16:25:24
It is my favorite ballpoint pen. Even though I think to buy it at the shop front, there are lots of types and it is troublesome, but it is convenient as I can ask while confirming. I'm buying it for something.
This review is about item#32906334.
Used to carry it to a notebook
4
From Japan
On 2015-05-20 15:11:00
I bought it as a replacement core of knock type uni-ball 0.38. It is easier to write and the thickness of the ink is 0.38 and it is thin so I use it in the notebook. I liked it so I was looking for a replacement core and bought it with "Monotaro". It was cheaper to purchase a new one because the shipping fee was high, but I purchased a replacement core because I do not want to increase the amount of waste in vain. If you correspond to mail service, the shipping fee will be cheaper and it will be saved, but I would like to continue purchasing if you can support it ...
This review is about item#32906334.
When filling in dedicated invoice with small letters
5
From Japan
On 2014-02-06 13:16:53
The pen tip is very solid and the characters are easy to write, it can be written smoothly without ink fade. It became one of my favorites.
This review is about item#32906334.
Bookkeeping
5
From Japan
On 2013-03-26 13:08:59
The pen tip is also thin and comfortable to write smoothly, so it is saved that there is a change of heart.
This review is about item#32906334.
1
Customer Who Viewed This Item Also Viewed
Uni-Ball Signo Ultra Fine
Uni-Ball Signo 0.28mm
Signino UMN-103 Light Blue 8
Ballpoint Pen Refill
Gel Ink Pen
Pen Replacement UMR-85N
Uni-ball UMN-103 Blue BK
Ballpoint Pen Refill
Knock Ballpoint Pens
Cremona rope scroll 6phi x 200m
Ballpoint Pen Refill
Mat for indoor
LOOK MAT