Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Brass Made Plug Coupler for Valve Type Medium Pressure

Brass Made Plug Coupler for Valve Type Medium Pressure
Sales Price: 6.99 SGD
Review Rating: 4.88
8 Customer Reviews
5 star 7
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
To piping of hot water circulation
5
From Japan
On 2018-05-16 19:04:52
I was impressed with the goodness of construction superior to what I had imagined. It is not inferior to the famous manufacturer NB article. It is saved because it is cheap. Durability will be verified with future use.
This review is about item#32976465.
Switching work of hydraulic piping
5
From Japan
On 2017-11-14 10:57:23
For now it is used confusingly with Nitto Kohki, but there is no leakage. I think that it is very good as a product.
This review is about item#32976447.
During machine maintenance
5
From Japan
On 2017-07-11 18:22:12
I am satisfied, as per the description of the item. I hope to utilize this experience in the future.
This review is about item#32976447.
As a connector of a vacuum circuit
5
From Japan
On 2017-01-18 08:39:58
I was satisfied with the performance which is inferior to anything expensive maker goods that I could purchase at a low price
This review is about item#32976456.
Thermic oil circulation of mold
4
From Japan
On 2015-06-26 15:31:51
Equivalent level to manufacturer products
This review is about item#32976474.
It is used for connecting the cow's aquarium.
5
From Japan
On 2013-07-08 08:10:57
I use it for connecting the cow's aquarium. When washing with water tank If you take away and wash it will install. It is in the place where the cow can lick but it does not take it with the tongue of the cow and it is strong and it does not leak, so I purchase it again.
This review is about item#32976474.
Stage change of cooling water pipe for stationary SW (spot) work
5
From Japan
On 2011-07-03 14:14:13
It was used for improving the step change of the cooling water pipe of the stationary SW (spot) work. Water pressure is 3 kg / cm 2, but it can be used without leakage. The desorption of water supply / drainage became very easy. Since we change the setup more than once on a day, it will be useful when we handle a lot of small varieties with one piece of equipment.
This review is about item#32976447.
Desorption of gasoline line
5
From Japan
On 2010-12-02 13:36:53
Adopted by switching the fuel line of gasoline engine bench, without leakage at pressure of 3 kg / cm 2 or more, reliable product because the material is also good.
This review is about item#32976447.
1