Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Linear Bush Straight Type

Linear Bush Straight Type
Sales Price: 4.99 SGD
Review Rating: 3.25
4 Customer Reviews
5 star 1
4 star 1
3 star 0
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
For vertical movement of work machine
From Japan
On 2015-10-11 18:50:46
I was purchasing because the play was attached to the thing which was attached from the former somewhat of the outline, but as I measured it with a caliper, it was 28 mm in external size so I thought that it could be attached without problems but the thing attached originally takes the ring Although it was missing, it was caught in a dent of the ring part to install this product, and it had to be entered unless it had to beat in with a driver + hammer.
This review is about item#32983203.
I use it in the moving part in a place where it wears (the shaft also works). It is also running in rotation and its perpendicular direction.
From Japan
On 2013-02-17 17:55:33
I am still planning it, so I use it in the test, but it is good if the shaft is a set. Movement, no problem. It works as expected.
This review is about item#32983133.
Self-made CNC
From Japan
On 2012-10-21 13:21:23
It is a good item due to the price. If you move grease and move it properly, it moves very smoothly. It is natural that grinding is not done in the state without putting grease ...
This review is about item#32983212.
Movable part of self made CNC
From Japan
On 2011-03-15 20:14:43
It did not become usable because it was rough running.
This review is about item#32983185.
Customer Who Viewed This Item Also Viewed
Linear Shaft
Linear Bush
Slide Unit
Simple Slide Bush, Sm Model
Linear Bush
Linear Bush
Linear bearing ECO-Series
Linear Bush
Double type slide bush
Linear Bush
Linear Bush Straight Type
Double type slide bush (SM - W type)
Simple Slide Bush, Sm Model