Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Deep Groove Ball Bearing No. 6900 ZZ C3 With Retaining Ring

Deep Groove Ball Bearing No. 6900 ZZ C3 With Retaining Ring
Sales Price: 5.99 SGD
Review Rating: 5.00
4 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Preliminary (o_ _) ノ 彡 ☆ ☆
5
From Japan
On 2017-04-13 03:11:36
Because it is an amateur. Because it did not understand what was somewhat even if it was told suddenly as a bearing. As I was told by a bicycle shop owner, when I searched based on "measured value", the more suitable products came out as it went bad. For the time being, it seems to be a daughter of a futo & a & ko choice that is slightly changed. So I did not use Kole after all. Because it is "preliminary" in the batting phase in which 200,000 bicycles are thrown away or thrown away. For me it is a gem that gave me a trusty big trump cardinality assurance ... Spup! O * - (ー ー ー ー ¨ _) y - ~ ~ ~ Pukapuka ~ In other words. The key factor I bought it! I wanted to buy this even though I was anxious after ordering conforming products, but as I added the shipping fee pretty much it will be a budget that goes beyond the scope of "preliminary" pretty much, so I thought I was going to misunderstand (· o ·;)! "The same day order is a shipping cost service (~ ^ o ^; No ~ \") as a sentence has jumped into the eyes so if you go back to service with a feeling of sorrow. Although it was treated as a separate item at a later date, it was really impressing that it was free, so it is a specimen that was impressed m (_ _) m
This review is about item#38374533.
Parts exchange of food manufacturing equipment
5
From Japan
On 2016-03-15 10:24:11
Half a year or more have passed since the exchange, but it can be used without problems.
This review is about item#33000335.
Substitution of lower arm for bush
5
From Japan
On 2015-04-16 14:49:34
It is used instead of a bush of a lower arm of a four-wheel buggy. I tried to buy a flanged to prevent the bearing from getting inside, but it is not a problem to enter but I plan to make the type without flanges next time.
This review is about item#33000335.
Part of machine parts
5
From Japan
On 2013-04-16 13:27:19
no problem
This review is about item#33000335.
1