Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of K Timing Pulley Pilot Hole Item XL037 Shape CF Type

K Timing Pulley Pilot Hole Item XL037 Shape CF Type
Sales Price: 5.99 SGD
Review Rating: 3.80
5 Customer Reviews
5 star 1
4 star 2
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Pulley change of electric sewing machine
5
From Japan
On 2017-10-18 23:00:41
Electric sewing machine thread breakage and needle bending continued more than before but suddenly the plastic pulley broke into two. When I was searching for a pulley of the same standard I was able to reach the perfect thing. Processing of the hole diameter and tapping of the set screw were necessary, but after replacement there was no timing deviation at all and a thick cloth became to be able to sew with no problem and it is satisfactory. Performance improved reliably.
This review is about item#33036385.
Table saw movement guide remodeling
4
From Japan
On 2016-04-23 07:52:47
Parallel to the cutting edge of the table saw, we made remodeling of the guide which is easy to move accurately at right angles. In order to move the guide in parallel, the two rotating shafts are synchronously connected. Purchased this pulley and timing belt. Dimensions of the pulley posted on the homepage were all written, so I got lost. Although a donut-shaped ring has a description to prevent coming off just by fitting, I do not understand well in sentences. I think that you do not need letters if there is an explanatory diagram.
This review is about item#33036385.
Alternative for motor pulley
3
From Japan
On 2016-03-17 09:42:20
Third-party products are integrally molded, but we chose it because the price is cheaper. I purchased it again because it can be used in the same way.
This review is about item#33036342.
For transmission of spindle rotation of mini machine tool
4
From Japan
On 2016-02-13 16:04:19
Although it is normal as a product, there is no problem, but if it is possible, it would be a good idea to have a pulley made of aluminum material, is not it possible to make it a bit cheaper in terms of price? .
This review is about item#33036342.
Used for manufacturing transmission of rotation of mini chuck of spindle
3
From Japan
On 2016-02-11 18:56:52
There is no problem as usual as a product, but it is saved if there is aluminum material if possible. If so, would not it be possible to make it a little cheaper in terms of price?
This review is about item#33036342.
1
Customer Who Viewed This Item Also Viewed
Timing Pulley MXL-, Army Type
Timing Belt XL037 Type
Synchro Pulley XL037 AF
Trapezoidal Tooth Pulley
Timing belt Model XL037
Timing pulley XL037 Model B
Timing pulley XL037 form C-shaped
Synchronization Belt Xl037 Type
Timing Pulleys XL Type
Trapezoidal tooth profile pulley XL
Synchro pulley XL037 form BF
Timing pulley Model XL