Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Suction Hose FW Type

Suction Hose FW Type
Sales Price: 37.99 SGD
Review Rating: 4.50
10 Customer Reviews
5 star 8
4 star 1
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Drainage suction work
5
From Japan
On 2016-10-29 17:01:56
Cheaper than home center. It is heavy, it saves the labor of going to buy it.
This review is about item#33051112.
Replacing old hose
5
From Japan
On 2016-10-14 13:23:59
It was cheaper than I expected. I wish I could exchange this amount earlier.
This review is about item#33051112.
Sludge suction of wastewater treatment
5
From Japan
On 2016-09-29 17:26:32
Nothing in particular. Packaging is simple and very easy to use.
This review is about item#33051094.
Used for pesticide spraying work
5
From Japan
On 2016-07-08 10:30:42
There is no particular problem.
This review is about item#33051112.
Sending milk
5
From Japan
On 2016-01-27 10:36:36
Although it is necessary for a worker to stepping on well, it is necessary to replace but if it raises the difficulty that it normally has sufficient function, although it is common, there is a feeling that the surface slightly felt immediately after purchase There is no problem other than that
This review is about item#33051094.
Used when φ30 PVC pipes must be bendable freely
5
From Japan
On 2015-09-21 22:15:55
When inserting into φ30 PVC, the suction hose is too dimensioned, spreading the silicone lubricant and inserting it while rotating it in the spreading direction. But, for now, there are no problems.
This review is about item#33051112.
Piping of pump
5
From Japan
On 2015-01-11 18:40:40
It is excellent in cost performance. Pump piping is sufficient strength.
This review is about item#33051094.
On the hose for the chiller
1
From Japan
On 2014-07-02 09:36:25
25 × 2 = 50 m is required, but limited to 5 m selling. There are similar products, but it is too expensive on 5th delivery.
This review is about item#33051094.
Pumping material (crushed plastic)
4
From Japan
On 2014-01-11 13:42:00
I would like to purchase the number of turns (5 m) in units of 1 m. Do not pull on the way (10m - 12m may be necessary)
This review is about item#33051112.
Pond water exchange
5
From Japan
On 2013-03-25 18:55:20
There is pliability in the hose, and there seems to be strength as well.
This review is about item#33051121.
1
Customer Who Viewed This Item Also Viewed
Suction Hose
Suction hose VS-A type