Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Dropper Bottle, Squareuare Type

Dropper Bottle, Squareuare Type
Sales Price: 5.99 SGD
Review Rating: 4.83
6 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Used for tapping
5
From Japan
On 2018-01-17 15:32:52
As a method of processing tap processing with oil less, a droplet Take the amount on the brush and apply it to the tap. There is no observation that a very small amount of a drop uses cutting oil, but a trace amount of film is also applied to the tap. This feeling is satisfied.
This review is about item#33148674.
For reagent
4
From Japan
On 2017-10-03 19:38:37
Container is solid, there is no problem. Although actually I wanted only the rubber part, I could not find that much sales, I bought each body. By all means, the eyedropper part of the rubber weakens over time. This is unavoidable for this. In this time, only eyedropper was removed, and the other part was discarded unfortunately. But it is a price that I can endure even though I think it is price of rubber from the price.
This review is about item#33148701.
Add a reagent just enough
5
From Japan
On 2016-05-01 14:43:48
It is thicker than the round bottle type and it is sturdy. Because the lid is also solid with a screw type, it has high sealability. Just because rubber is so, deterioration is quick when acid etc. are put in for a long time.
This review is about item#33148692.
When analyzing, when putting 1 or 2 drops of reagent.
5
From Japan
On 2015-12-06 20:13:35
Because the price was cheap, I ordered with no good, but I am very satisfied. It is really convenient to put 1 or 2 drops of reagent.
This review is about item#33148674.
Aqua water tank conversion
5
From Japan
On 2015-12-02 00:59:59
Used for Contra Kororain etc. when converting a tank. With a single siphoning, it is almost 1.2 ml so about 7 L of chalky-free.
This review is about item#33148692.
To put chemicals
5
From Japan
On 2014-01-31 13:51:07
Because it is a bottle with a heavy feeling, it is also a good point to collapse. Even if you carelessly hit it is okay.
This review is about item#33148717.
1
Customer Who Viewed This Item Also Viewed
Dispensing Bottle, Pump
Dropper Bottle
Mini Standard Capsule
Eyedropper bottle
Dropper bottle
Polypropylene bottle
Poly drop bottle 1.5 mL milky white
Eyedropper bottle
Keepore A
Spoid Bottle, No Rubber
Dropper bottle
Eye Drop Bottle, No Rubber Cap
Glass Pigment Bottles