Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Cork Stopper

Cork Stopper
Sales Price: 12.99 SGD
Review Rating: 4.57
7 Customer Reviews
5 star 5
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
As a test tube lid.
From Japan
On 2017-12-12 18:50:45
I was looking for a cork of a size suitable for the test tube purchased at another shop. Because there are many different sizes by shops in detail, which do not know what size you are looking for, what you are asking for if you do not care if you do not get in your mood What to do If you do not add it too much Why do not you try too much Why do not you fall into it Size checked many times on various sites I played afterwards. The condition is also exquisite and beautifully settled and I am very satisfied. It was good as I could buy it when it was cheap before it gone.
This review is about item#33465442.
Let's make the reflector of the shinko flute mouth.
From Japan
On 2017-03-02 17:53:41
It is better if there are various thicknesses (separately for 20 mm / 19 mm / 18 mm / 17 mm of the thickest portion)
This review is about item#33465223.
As a plug of a glass bottle
From Japan
On 2016-11-27 09:13:56
Both size and flexibility were appropriate, and it was possible to use it without any problem with the desired product
This review is about item#33465257.
Inside of the flute
From Japan
On 2015-09-15 17:51:36
I think that it was good.
This review is about item#33465582.
Used as part of production product
From Japan
On 2015-05-02 01:10:11
Various sizes are available and very convenient to use
This review is about item#33465372.
Used as a lid by making accessories
From Japan
On 2015-04-12 17:07:10
I got a lot of sizes so I can use them separately and it is very convenient to use.
This review is about item#33465293.
Bottle bottle cork
From Japan
On 2013-04-09 14:44:46
When making blue sunny waters, water may expand and faucets may fly, but cork stoppers are breathable so it is convenient in such a case.
This review is about item#33465406.
Customer Who Viewed This Item Also Viewed
Cork Stopper
Silicon Plug
Test Tube Culture
P-Test Tube Straight Mouth
Cork Borer
Silicon Plug
Silicon Rubber Plug, Color
Non-Combustible Plug
Glass liquor bottle
Natural cork Kawasen
Screw Cap Test Tube
Round (round bottom) tube
(18571) cap, the canister air
Cork Stopper